STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LL USART APIs not woriking!

Posted on June 07, 2018 at 08:33Dear friends,I am trying to send data over RS485 protocol using a STM32F107RCt6 MCU.I config the project in CubeMX and when I write the following code, the USART does not send any data while the project compiles succe...

Mujtaba by Senior
  • 1079 Views
  • 1 replies
  • 1 kudos

Enabling UART Idle line interrupt causes program to hang

I'm using STM32L062K08 MCU with HAL library. I found out setting idle line interrupt causes program to hang. It worked when I used for UART2. __HAL_UART_ENABLE_IT(&huart1, UART_IT_IDLE);  // enable idle line interruptWhat could be the possible reason...

Ash G by Associate II
  • 1033 Views
  • 1 replies
  • 0 kudos

Resolved! How to write to RTC backup registers on STM32L433 ?

Is there something else that I am missing? I have followed the instructions in UM1884 and RM0394, but after writing to BKP0R, it still reads zero (even with NoErase).0x40021058: 1006c401 1 RCC_APB1ENR1_PWREN 0x40007000: 00000300 1 PWR_CR1_DBP 0x4...

Resolver for STM32F4

Hello everyone. I'm working on a project. I must use a resolver for our servo motor. But I could not find any sample code for resolver.Can anyone help me?Thank you.

Mert by Associate
  • 3946 Views
  • 7 replies
  • 0 kudos

Voltage problem on VDD pin on SWD connector.

It's my first design with a STM32 MCU. I want to program a MCU on my custom board with the ST-LINK but when I try with STM32 ST-LINK Utility the connection doesn't work. The STM isn't recognized. When I measure VCC signal on the connector SWD I have ...

Resolved! STM32F439NIH can't get PLLCLK on MCO1 (solved)

Posted on February 17, 2017 at 12:29I want to have 60 MHz on the MCO1 pin PA8. I use an external 25 Mhz crystal. The PLL delivers 180 Mhz to the system clock. I've used STCubeMX to configure the clocks to get 180 MHz / 3 on MCO1.Unfortunatly I'm not...

lasse by Associate II
  • 1404 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.