STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Help me choose MCU

Hello guys, I am building a product, actually am migrating my product from ATmega to STM MCUs, my requirements exactly are as follows,Cortex M0 or better core, >48 MHz2 Channel 5V DACs1 Channel CAN for OBD2 Interface2 Channel ADCs, at least 10 bit re...

Resolved! stm32f746 sdmmc 1 Bit vs 4 Bit Data

Designing custom board based on STM32F746G-DISCO.  I am using the TQFP chip, so a few less IO.   The DISCO board uses a 4 wide data, but I do not have enough pins so I will only have 1 bit wide data.  I only want to use SD card to be able to upload n...

FJB2069 by Senior
  • 3272 Views
  • 9 replies
  • 1 kudos

Resolved! LTDC configuration on STM32F469

@Tesla DeLorean  Hi! I wonder if someone can help me! I am trying to initialize a LCD screen and I have some questions. I am using a STM32F469IIT6, and it does not have enough memory in itself to hold a buffer for my screen 800x480. I did not set up ...

Resolved! Getting started with STM32 - Basic questions

Hello, As a newbie to STM32 , Could some experts please answer these questions for meIs there any basic documentation that provides an overview of what software i will be needing installed on the PC? This is what is my understanding so far, there is ...

ak52 by Associate III
  • 2944 Views
  • 6 replies
  • 3 kudos

Powering stm32g051f8 from LiPo battery

Hello, according to the datasheet of stm32g051f8, the absolute max power supply voltage is 4V but the fully charged 1-cell LiPo battery Voltage is 4.2V. Can I power this MCU directly from the battery?

HDKLog by Associate
  • 1348 Views
  • 3 replies
  • 0 kudos

Resolved! Flash drive in Nucleo-F446RE

Hello,When I plug this board to my computer, appears a removable disk of 1,6 MB capacity.Is this disk accessible from the MCU? For store small data, or make a dataloggerWhere the filesystem is stored? Neither the STM32F446RE nor STM32F103CB of the ST...

xisco by Senior
  • 4315 Views
  • 9 replies
  • 2 kudos

QUADSPI_BK1_IO3 issue in STM32G474 and STM32H753

Hello.I am testing QSPI indirect mode using STM32G474 and STM32H753.However, I found a weird operation of QUADSPI_BK1_IO3 pin.Other pins are OK, but QUADSPI_BK1_IO3 is high states as in the redboxes.It should be low states (0).I have tested in STM32G...

junggun_1-1720156873124.png junggun_2-1720157273932.png
junggun by Associate
  • 2771 Views
  • 5 replies
  • 0 kudos

Resolved! STM32 Black Pill not working with clone ST-LINK V2

Hello everyoneIt's my first time messing around with STM32 microcontrollersA few days back I got a black pill (STM32F401CCU6 - https://robu.in/product/stm32f401ccu6-minimum-system-board-microcomputer-stm32-arm-core-board/) and an ST-Link V2. The blac...

MihirJ by Associate II
  • 7127 Views
  • 5 replies
  • 1 kudos

LAN8742A PHY: Unstable Ethernet at 100 MHz

Hello STM32 world!Here are a few words to share our issues—now resolved—with the LAN8742A Ethernet PHY.We designed a board based on the STM32H573, featuring an Ethernet interface.We strictly followed the design used in STM32 boards, particularly the ...

Charlu31 by Associate
  • 1337 Views
  • 1 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.