STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! DMA transfer error in STM32H7 DCMI

Hi all,I am trying to setup a DCMI example with NUCLEO-H743ZI, the DCMI interrupts work fine, but DMA abrot when transferring the first data and TEIF is set.The project was setup with CubeMX, and more detail changes is in the git log. I didn't use ca...

i0x0i by Associate II
  • 3871 Views
  • 5 replies
  • 0 kudos

Resolved! Can't download the x-cube-eeprom libary form st.com

I tried to download the x-cube-eeprom libary for the stm32l4 devices.When press the "Get Software" button on the https://www.st.com/en/embedded-software/x-cube-eeprom.html site nothing happens when im logged in to my account

eSchm by Associate
  • 3069 Views
  • 2 replies
  • 0 kudos

Resolved! Regulation & license for product Nucleo

Hi there!​We are using nucleo embedded board for one of the application in IOT. We could like to sell this product to end customers, so is there any rules & regulation which we have to follow to sell this product.​​​

MMyla by Associate
  • 1155 Views
  • 1 replies
  • 0 kudos

Micron® Memory Support for STMicroelectronics®

Has micron eMMC memory support been released for stm32 platforms? there is nothing but this document. https://www.micron.com/resource-details/41f6ea73-754f-45f6-8039-2e19f5394ca8reference design, sample code etc.We want to read and write micron MTFC ...

akesk by Associate II
  • 1190 Views
  • 1 replies
  • 0 kudos

Resolved! CAN Interrupt not firing on STM32F072

I am using a mixed LL-HAL setup on an STM32F072 target. Although the HW transmits a CAN message using HAL_CAN_Transmit_IT(), it appears that the CAN interrupts do not execute. There seem to be two-ish parts to this problem:(1) The Main interrupt ha...

NPol by Associate
  • 2585 Views
  • 3 replies
  • 0 kudos

One pulse mode

Hello everyone.I'm studying in stm32f40g eval and using timer in one pulse mode.First I'm use the example code TIM_OnePulse and modify it. I'm add the One pulse OUTPUT in function TIM_Config and One pulse EXTERNAL TRIGGER in function TIM_T2IConfig. I...

How migrate STM32L432KC MCU to STM32L452RE MCU?

How can we provide support to two devices (startup files) for a developed application. I am using STM32L432KC MCU and i want to migrate my application to STM32L452RE MCU. Is there any way to do the same?

Niks by Associate II
  • 1346 Views
  • 2 replies
  • 0 kudos

Resolved! STM32f746G - Discovery - Audio Pins

Hi I am having issues with playing sound through the audio out jack. I have gone through the BSP examples but what's lacking for me is the correct setup of the pins. At the moment I have set up -SAI2 Block A (Master) - (I2S/PCM enabled)I2C3 I2S3 DMA ...

Avan.7 by Associate II
  • 1217 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.