STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F091 ADC DMA problem

Problem with ADC reading at 100 kHz via DMA.MCU runs @ 48 MHz, ADC @ 14 MHz. Configured via CubeMX.Trying to read one ADC channel (1.5 cycles), triggered by Timer 15 (100 kHz) using HAL.Cannot reach 100 kHz (see pictures)​. Blue are DMA interrupts (h...

JuM by Senior
  • 1898 Views
  • 4 replies
  • 0 kudos

Not detecting the usb device in Dfuse

I am trying port sample code via usb fs of STM32H743 MCU. I have installed dfuse in win7. But my device is not getting detected. In deVice manager I see warning mark on STM device in DFU mode. If i check the details, it says digital certificate is no...

STM32F746G Sampling Error

I use the BSP functions to record audio. The sampling frequency is set to 8000 Hz and the buffer size to save the recorded data into is set at 8000 elements long. It would make sense if the time to fill up the buffer is 1s. However it takes exactly 5...

Avan.7 by Associate II
  • 1676 Views
  • 3 replies
  • 0 kudos

Need to hide the .c files from client

I have been using Atollic TrueSTUDIO for STM32F3DISCOVERY applications to write and test algorithm for a client. After successful debugging and testing I have to handover the project to the client. However I cannot reveal my source code which is actu...

ARauf by Associate
  • 2567 Views
  • 4 replies
  • 0 kudos

send message to Sigfox cloud

I bought  Discovery kit for LoRaWAN™, Sigfox™, and LPWAN protocols with STM32L0 . Then I read https://github.com/aureleq/muRataSigfox . This is about my same kit. I was able to register it with Sigfox. More, I read http://blog.aha.nl/2018/02/getting-...

ATrev by Associate II
  • 1114 Views
  • 0 replies
  • 0 kudos

Unexpected values of variables in STM Studio

Hello,I have been using STM studio for monitoring run time behavior of a software for STM32F4 and I have noticed that traces of some variables contain abrupt changes to zero value. The zero values are displayed despite the fact that the actual value ...

0690X000006BsKaQAK.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.