STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to measure power consumption for Nucleo-144 board?

I am trying to measure the power consumption for Nucleo-144 board.Here is my configExternal power supply 8VJP6 to VINConnect Fluke multimeter to power supplyConnect multimeter to CN8 pin 15Connect ST-LinkCall HAL_PWR_EnterSTANDBYMode() or LL_PWR_SetP...

External Power supply configuration for L432KC nucleo

When I power my nucleo through the 5V pin, with a 5V supply, the behavior of the controller is not normal. If I power it by USB, it works well. I read the User Manual, have I misunderstood something? What could be happening?

xpp07 by Senior
  • 1305 Views
  • 5 replies
  • 0 kudos

Resolved! Is there any documentation on the updated HAL_Can Library?

Hello, I was trieng to use STM32Mat (with simulink) and came across some errors.I discovered that the HAL Library was updated but the STM32Mat wasn't.I'm willing to code everything by hand without using Simulink but I would need documentation on the ...

STM32f303k8t6 Nucleo board with DS18S20 Temp sensor.

Dear all, I want to read the temperature by DS18S30. For that I have downloaded the library for DS18B20 (not DS18S20, because not available) from https://github.com/nimaltd/ds18b20. I have added this to my project in Keil as shown in figure. But it c...

0690X000006BtcRQAS.jpg
ssaho by Associate
  • 1028 Views
  • 1 replies
  • 1 kudos

Does STM32H7 support ISO CAN FD?

The Reference manual states that the FDCAN supports CAN FD according to specification 1.0, but also states it is ISO 11898-1:2015 conformant.Also: There is a bit in one of the control registers that suggests the FDCAN can support both versions. Is th...

FGutm by Associate
  • 1116 Views
  • 1 replies
  • 0 kudos

STM32F411RE using External power supply

Hello,to finish my project i want to remove my the cable wich is plugged in to my PC. So i need an external power supply. In the Datasheet i found the topic "external power supply" but i still dont know how to connect it. It says that i have to use E...

How to interface STM32F429IGT with an external SDRAM?

Hi,I’m trying to connect an external SDRAM (part no. K4S561632N) to STM32F429IGT. For that, I am using STM32CubeMX to generate the code. Shown below is the initialization and configuration of the external SDRAM:The IDE that I am using currently is Ke...

0690X000006BtmWQAS.png 0690X000006BtmbQAC.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.