STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L4R9I-EVAL OctoSPI problem with 8bit access

Posted on May 19, 2018 at 22:56Hello,I am currently using the OctoSPI RAM on the STM32L4R9I-EVAL board (IS66WVH8M8BLL-100BLI (Hyperram)).At first sight everything looks as expected, but when I read and than write with 8 bit access, only every second...

s m by Associate III
  • 4301 Views
  • 9 replies
  • 1 kudos

Analogue input 40mv out.

Hi I am using a stm32L433 100 pin with an external 2.5v reference chip connected to vref+. I have tried placing a voltage (tried different values) onto one of the a/d channel, but the result is 40mv low. I then programmed the D/A , which uses the ...

Error instantiating RTE components Error #542: API '::Board Support.LED:1.0.0(API)' required by component 'Keil.STM32F4-Discovery::Board Support:LED:2.0.0' is missing

I'm using Windows 10 and arm KEIL IDE along with STM32F407G-DISCOVERY board. I'm a very beginner and trying to do something with LED. I'm stuck at the initial stage itself. I have a problem with the LED API in the Board Support Package in the set...

0690X000006Bw2fQAC.jpg
RVarm by Associate
  • 3552 Views
  • 3 replies
  • 0 kudos

Glass LCD STM32L0

Posted on April 13, 2016 at 23:25Hi,I facing problem with custom segment glass LCD interfacing which include 4 COM pin and 20 SEGMENT pin with 1/4 duty cycle and 1/3 bias (Refer Attachment).I tries to understanding HAL library provided on ST site ex...

bhavesh by Associate II
  • 1657 Views
  • 1 replies
  • 0 kudos

ADC and Asynchronous clock mode?

Hi guys. I designed a simple PCB for measuring the battery voltage of a biomedical instrument. But I faced a simple problem. I use HAL to generate the code. So when I set the ADC clock in Asynchronous clock mode the while(1) is not executed!!!IS it b...

Resolved! Wrong value of VCAP capacitors in STM32F407VGT board

I have 10uF (=10uF+100nF)ceramic capacitors for VCAPs in a custom board. Voltage there is 2.7V. Supply voltage is 3.3VI have problems getting the STlink to accept the board. First I managed to erase the chip, now STLink does not even recognise the c...

LMI2 by Lead
  • 4504 Views
  • 10 replies
  • 0 kudos

Is Full Duplex Possible with DMA and how to use it with CubeMX

Hello there,up to now i have used an Audio DAC on a STM32F407 with DMA and Half/Full Transfer Interrupts with CubeMX. So far so good.But now i am a little bit confused. As i have read some Posts it seems that it might be not possible to use Full Dupl...

RBoel by Associate
  • 1960 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F7X internal regulator won't start

hello I am using the STM32F779NXH MCU it has an internal 1.2V voltage regulator that I believe should output volt on the CAP_1 and CAP_2 pins. The MCU will not boot, and will not be recognized by the st-link. This is a brand new board and has never ...

TallGUY by Associate II
  • 2203 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.