2018-08-24 7:53 AM
Hi
I am using a stm32L433 100 pin with an external 2.5v reference chip connected to vref+. I have tried placing a voltage (tried different values) onto one of the a/d channel, but the result is 40mv low. I then programmed the D/A , which uses the same VREF+ and tied it to the input channel of the A/D. The value on the D/A is what I expect, but the A/D channel is still reading 40mv too low. Anyone any idea what this may be?
Many Thanks
Scott
2018-08-24 11:39 AM
Missing or incorrectly performed ADC calibration (e.g. during VREF source startup or violated ADC voltage regulator startup time)? Too high signal impedance plus too short sampling time?
JW
2018-08-24 1:04 PM
As I am using an external VREF (I have connected a 2.5v reference chip), I never done a calibration as I thought it was only for internal VREF?
Thanks
Scott
2018-08-24 1:38 PM
Okay, and if you stop thinking that?
JW
2018-08-24 11:50 PM
"Okay, and if you stop thinking that?" , what does that mean?
I added the calibration and it worked, I just thought this was for calibrating the internal VREF when not using an external reference.
Thanks
Scott
2018-08-25 1:36 AM
> "Okay, and if you stop thinking that?" , what does that mean?
That was in reply to your previous:
>> I never done a calibration as I thought it was only for internal VREF
trying to suggest to do calibration which you did and it apparently helped. Please mark thread as resolved.
JW
2018-08-25 9:29 AM
It works well, I simply thought when using internal reference voltage this needed but not when using an external reference voltage
Scott
2018-08-25 9:31 AM
How do you mark the thread resolved?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.