STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is there an emulator software by STM Microelectronics or 3rd party for STM32L476VG (with or without the discovery board)?

We want to test the performance of our algorithm on this platform, and it would help if we can do it in an emulated environment before flashing to the real board, so as to save the time of re-flashing every time. For example: the GNU MCU Eclipse as d...

CPath by Associate
  • 883 Views
  • 0 replies
  • 0 kudos

Issue to use SPI1 with port B GPIOs

Hello All,What is the secret to enabling SPI1 on PortB GPIO? Attached code below works fine on GPIOA bits PA5 and PA7Any ideas?Thanks in advance,MikeLifting the example straight from the reference manual....// Configure PortA bits 5 and 7 for alterna...

uart rx interrupt advice

Hi All,I'm after a little bit of advice on how to use the uart interrupts. I would like to implement an interrupt driven uart receiver which takes a single byte at a time and stuffs it into a buffer. When a terminating char is received, a flag is r...

Non unique unique device ID or counterfeit parts?

Hi,I've encountered with weird situation with STM32L053C8T6 devices, namely all the devices share the same unique device ID. I use LL_GetUID_WordX() functions. And for the third word (LL_GetUID_Word2), I tried both offsets, 8U as current Cube library...

Innomatic by Associate II
  • 1263 Views
  • 4 replies
  • 0 kudos

Nucleo F767ZI: How to interface OV5642 Camera ?

Synchronization failed between OV5642 module Camera of Omnivision and Nucleo F767ZI (STM32F767ZI). Fail the VSYNC and HSYNC Signals.¿How could i implemented the camera on Nucleo F767ZI through DVP Parallel interface? I have a problem with the synchro...

I2C between 2 stm

Hi.I want to communicate between two stm32 of different cores via I2C, lets say between F0 and F7.F0 would be slave and F7 master.The idea is when user button on F7 board is pressed ,the control will shift to F0..but i don't know how to give a slave ...

asim khan by Associate III
  • 734 Views
  • 0 replies
  • 0 kudos

SMT32F1 I2c SCL stretching

Hi, allI have a project using a STM32F103c8t6 that works perfectly with HAL 1.4.0, but when I update a HAL to 1.6.1 version, the i2c device which is configured as a slave, after some writing or reads from the HOST it keeps the SCL in LOW, causing acc...

CBair by Associate
  • 684 Views
  • 0 replies
  • 0 kudos

pinout for stm32f429

hello I'm looking for a pinout for board stm32f429, a pinout that shows how the LCD tft (ili9341) is set to which pin on the board.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.