STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Understanding STM32 Sub-families

I have selected the STM32F091RCT for a new design and was having trouble understanding a specific section of the naming schema -Example: STM32F091RCTSub-family: '91'0: Value line1: Access line2: USB line8: Low-voltage lineThe '1' makes sense this is ...

Justin1 by Senior
  • 1855 Views
  • 2 replies
  • 0 kudos

STM32L452RE Nucleo Board

​Based on STM32L452RE specification, it can support from 1.71V to 3.6V. I have try using external 3.3V power supply to power up the board. Q1, However when I change the voltage from 3.3V down to 1.8V, the reset signal voltage level change. At this po...

ychua by Associate
  • 745 Views
  • 2 replies
  • 0 kudos

Ethernet IAP doesnt work with newer browsers. How to fix?

Hello, I got the IAP example running and found that it does not work properly with newer browsers (i tried Chrome, Firefox, Edge, all of newest version). The index page loads fine, but when the user and password is posted, the upload page does not lo...

Thomas K by Associate II
  • 2028 Views
  • 5 replies
  • 0 kudos

S2-lp 868Mhz

I are using LDC RX s2lp mode.With news, but brand TM thương mại TX?Thank you. Tôi đến từ Việt Nam

DNguy.2 by Associate
  • 748 Views
  • 0 replies
  • 0 kudos

Using STM32F427 bootloader with canbus

Hello!We have custom board build with STM32F427 and embedded linux and i am trying to connect the STM32 bootloader with canbus. On the board the STM32 uses CAN2.I can toggle the pins BOOT0 and RESET from the linux, and i can program the stm32 fine wi...

PSalm by Associate II
  • 3132 Views
  • 5 replies
  • 1 kudos

RTC not functioning correctly

Hi Community,I have 2 Lora loggers (with the exact same code) running and capturing the transmission from Lora sensor units.Every transmission is time stamped by the logger. If you look at the image attached, you'll see the logs of the 2 loggers. If ...

ANair.19 by Associate
  • 1545 Views
  • 2 replies
  • 0 kudos

PINRST seems to be always set

It seems PINRST is always set, even if the reset is caused by me removing the IDD jumper. How do i distinguish between this and a reset caused by pressing the reset button?

G5658 by Associate III
  • 659 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.