STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-SMCARD issue

Dear,I designed my own board similar to STM3210B_EVAL.I built the X-CUBE-SMCARD project and programmed it on my board.The smart card that I use, response to ATR, but no response and no Ack to another commands ( same as Select File ,...)how can I deb...

RTC and Alarm subsecond mask

Dear,I want to use an Alarm A in RTC mode. But have some trouble with it.1) I use LSI 37000 Hz2) for 1 Hz I selected PREDIV_S=7399 and PREDIV_A=4It means that my Granulanity is 1/(7399+1)When I want to wakeup for example in 100 ms.1) I read actual ...

JAN R by Associate III
  • 2049 Views
  • 3 replies
  • 0 kudos

Resolved! STM32 HAL I2C Driver - Wrong Slave Address

Hi, I have a board with STM32F501R8T6 and AT24C02 & DS1307 RTC are connected to I2C2. Earlier i had used custom I2C driver and interfaced them with a 8051 controller without any issues. Now since there is a need to change the I/0 pins config in ARM ...

PR.19 by Associate II
  • 1865 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.