STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Sampling a signal from brigde ?

Dear ST Community Members,I'm using ST Nucleo and STM32CubeMX, and want to sample an output signal from bridge rectifier,it has 100Hz Freq, I'm thinking in between peak, I sample 10 times ?Any method or ideas ? I use ADC0 or ADC1 for this purposeThan...

ADC value on multiple channel ?

Dear Member,I have a question related with multiple channel on ADC ,how can I retrieve the value of channel 1 and channel 3,4 and 5 fromadcResult= HAL_ADC_GetValue(&hadc); ?RegardsBianchi

STM32L053C8, problem with standby mode and wakeup pin

I am using an STM32L0C8T6 MCU and STM32CubeMX to generate the hal driver for my first project. One of the features of the project, is to configure it to go into standby mode to conserve lowest power consumption if my program is idling for some amount...

SKoh.14 by Associate
  • 862 Views
  • 0 replies
  • 0 kudos

Resolved! Best processor selection

Hi,I am trying to select an STM32 for a project but am struggling a little with the selection tables and thought I would check to see if there is an easier way before I spend hours on repetitive tasks.My fundamental requirements are: 2 x ADCs (indepe...

AClif by Associate III
  • 3238 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.