2018-11-06 7:55 PM
I'm testing my small project using SPI.
In that project, the board, Nucleo-L432KC (used as a mbed board), has to receive data from a SPI master as a SPI slave, and send processed data to another device as a SPI master.
Then, the board has to work as a SPI slave and a SPI master at the same time.
Nucleo-L432KC has 2 SPI (SPI1 and SPI3) and so I tried to configure both of them, but SCLK output as a master didn't work.
Is it possible to use 2 SPI as a master and a slave?
Configuration
SPI1 as a slave
using MOSI = A6, MISO = A5, SCLK = A4, SSEL = D3
format:(8,3), frequency:6750000
SPI3 as a master
using MOSI = D11, MISO = D12, SCLK = D13, SSEL = D9
format:(8,3), frequency:6750000
If they are not configured at the same time, it seems to work well.
a part of my code:
SPI_3_SSEL = 1;
spi_3.format(SPI_3_BITS, SPI_3_MODE);
spi_3.frequency(SPI_3_FREQ);
SPI3->CR1 &= ~0x80; //MSBFirst
spi_1.format(SPI_1_BITS, SPI_1_MODE);
spi_1.frequency(SPI_1_FREQ);
SPI1->CR1 |= 0x80; //LSBFirst
SPI1->CR2 |= 0x40; //Interrupt
NVIC_SetVector(SPI1_IRQn, (uint32_t) &intrrptSPI1); //Callback function
NVIC_SetPriority(SPI1_IRQn, 1); //Priority
NVIC_EnableIRQ(SPI1_IRQn); //Enable interrupt
2018-11-06 11:01 PM
> If they are not configured at the same time, it seems to work well.
Read out the content of SPI and relevant GPIO registers - both when configured separately and working, and when configured together and not working - and compare them.
JW
2018-11-06 11:41 PM
Thank you for your advice!
I checked SPI registers and they were following.
only SPI1
SPI1 CR1:00db
SPI1 CR2:1740
SPI1 SR:00c2 or 0082 or 0042 or 0002
SPI3 CR1:0000
SPI3 CR2:0000
SPI3 SR:0000
only SPI3
SPI1 CR1:035f
SPI1 CR2:1700
SPI1 SR:00c2 or 0082 or 0042 or 0002
SPI3 CR1:0000
SPI3 CR2:0000
SPI3 SR:0000
both SPI1 and SPI3
SPI1 CR1:00db
SPI1 CR2:1740
SPI1 SR:00c2 or 0082 or 0042 or 0002
SPI3 CR1:0000
SPI3 CR2:0000
SPI3 SR:0000
(The value of SPI1-SR changed at each trial.)
It implys that SPI3 is not used??
I thought the number of SPI is determined by PIN number for MOSI, MISO, SCLK, but that's wrong?
In my code, I define SPIs as following.
const int SPI_3_BITS = 8;
const int SPI_3_MODE = 3;
const int SPI_3_FREQ = 6750000;
const PinName SPI_3_MOSI = D11;
const PinName SPI_3_MISO = D12;
const PinName SPI_3_SCK = D13;
DigitalOut SPI_3_SSEL(D9);
SPI spi_3(SPI_3_MOSI, SPI_3_MISO, SPI_3_SCK);
const int SPI_1_BITS = 8;
const int SPI_1_MODE = 3;
const int SPI_1_FREQ = 6750000;
const PinName SPI_1_MOSI = A6;
const PinName SPI_1_MISO = A5;
const PinName SPI_1_SCK = A4;
const PinName SPI_1_SSEL = D3;
SPISlave spi_1(SPI_1_MOSI, SPI_1_MISO, SPI_1_SCK, SPI_1_SSEL);Thank you in advance
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.