STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Reinitilaization of ADC3 in DMA mode not working

Hey Guys,Iam using a STM32F429IDISCOVERY board with ADC3 in dma mode. Sometimes on special usage circumstances ( a lot of stuff is happening in parallel) there is an overrun error, because the processor is not fast enough to get the packages. Normall...

Switch over RTC from LSE to LSI while running

Hello all!Using STM32L433, RTC is initialized with LSE, works fine.In run, I want to switch to LSI and do certain steps and want to get back to LSE. What is the way to switch over RTC source LSE<->LSI ? I read some thing about backup domain. Please g...

SPate.7 by Associate
  • 2459 Views
  • 3 replies
  • 0 kudos

Compatibility for stm32l031f6 with STMFlashLoader.exe

Hi, I am currently using the stm32l031f6 which is a 32K memory device and I am trying to use the STMFlashLoader.exe, which is the command line version of the flash loader, to download firmware into the device. However, in the map directory for the ST...

MGan by Associate II
  • 2793 Views
  • 5 replies
  • 0 kudos

How detect SD card with external interrupt ?

Hi,I generated code for SD card and FATFS with CubeMx for STM32F407.How do I use BSP_SD_ITConfig (), BSP_SD_DetectIT () and BSP_SD_DetectCallback () to detect the presence of SD. I have found no example anywhere.Thank youPeter

Peko by Associate III
  • 1115 Views
  • 1 replies
  • 0 kudos

DFU USB and USART are not getting in some boards

Dear ST Team We are using STM32F765IGT6 in our design in a lot of 10 cards ,6 cards are not able to detect DFU and USART1/3 in boot mode.After programming they are giving proper console at USART 1 as per my design. Kindly suggest some debugging ste...

PKuma.0 by Associate
  • 1732 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.