STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 F4 USB FS Host: CDC device plugged before device start

Posted on July 27, 2017 at 15:27Hello,we are using the USB Full Speed host port on an STM32F4 with FreeRTOS.We use the most recent libraries:- stm32f4xx_hal_hcd.c stm32f4xx_hal_hcd.c and stm32f4xx_ll_usb.c version 1.7.0- CubdF4 niddleware STM32_USB_...

h p by Associate III
  • 2698 Views
  • 4 replies
  • 0 kudos

I2S Data stored in .wav file not playing correctly!

Hi I have ADAU1978 which is a quad ADC that gives I2S data which im trying to store in a SD card under .wav extension. When i do this i get a .wav file of size 8kB. When i try to play it with windows media player, it doesnt throw any error,but doesnt...

Resolved! I2C clock timing generation

Hi,I've read that for some STM families (F0, F3, L0, L4, etc.) the I2C clock timing must be calculated with an excel file or with the STMCubeMX software.The calculus is "closed source"? Can I reproduce it in my own code?I'm writing an interface for a...

Resolved! Do we have example codes on how to use fire wall to protect function on Flash and data on SRAM for STM32L073RZTx micro controller ? please share the link

I am trying to protect code(in flash) and data(sram) using fire wall feature But board is resetting when exucute the function. Following is the code to initiate and enable fire wall. void firewall_init(void){ FIREWALL_InitTypeDef firewall1; firewall1...

sMNMS by Associate
  • 1590 Views
  • 2 replies
  • 0 kudos

MEM-to-MEM transfer using DMA (SRAM to FSMC/FMC)

Hi,As far as I remember, I've read something about that a while back. I was wondering if I can send data to a memory-mapped device (FSMC/FMC) in a continuous loop a byte per iteration using the DMA peripheral. Thanks

Zaher by Senior II
  • 1355 Views
  • 2 replies
  • 0 kudos

STM32F10x entering standby mode fails occasionally

Posted on October 28, 2016 at 02:11We use PWR_EnterSTANDBYMode library function to enter the standby mode. I have added line to enable WKUP pin. The STM32 enters standby mode most of times. But, sometimes(once in 25 or so times), it just reaches the...

sandeshm by Associate
  • 15277 Views
  • 9 replies
  • 0 kudos

STM32L486 mcu used as Master SPI, Zigbee device as slave. What configuration of SSM and SSI should i be using?

I am going through an existing implementation, where my MCU's(STM32L486) SPI1 (PA4(NSS), PA5(SCK), PA6(MISO), PA7(MOSI) is used as master, the slave device is a zigbee stack.Currently the master's SSL is configured as Software managed, (SSM=1, SSI= ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.