STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Do we need to enable and set SVCall, PendSV priorities ?

Hello,In stm32cubemx generated code there is the following routine.void HAL_MspInit(void) { /* USER CODE BEGIN MspInit 0 */   /* USER CODE END MspInit 0 */   __HAL_RCC_SYSCFG_CLK_ENABLE();   HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_4);...

ranran by Senior II
  • 1229 Views
  • 0 replies
  • 0 kudos

USE MCU LIKE PL2303A

Hi everyone!How can i use my MCU STM32F407IG like a PL2303 FTDI. Like basically how can i use my mcu as a usb to uart converter? I already worked with the usb device cdc example and i send data to uart tx everything is fine an working but somehow wha...

arduo by Senior
  • 2032 Views
  • 6 replies
  • 0 kudos

No Space in execution region with .ANY

Hi,I am working for an project with STM32L496 target board. When i tried building the project, i got the error saying,ERROR: L6406E : No Space in execution region with .ANY main.o(.bss).I am trying to use full SRAM memory present(320KB) for the globa...

rsoma by Associate II
  • 6803 Views
  • 6 replies
  • 0 kudos

How to connect the bankselect pin to SDRAM device.

hello! i am using stm32f429 mcu ,i want to add a sdram as the main RAM.My sdram detail informatin,512K Words x 16 Bits x 2 Banks.i donn't know how to connect the pin which connect to sdram and control the internal bank of sdram to the sdram.s...

jxued by Associate
  • 645 Views
  • 0 replies
  • 0 kudos

Debugging a hard fault on STM32F405RG

Hello,I'm having a hard time debugging a hard fault I'm experiencing.The hard fault occurs in the handler of external interrupt. Here's it's code:extern "C" { void EXTI2_IRQHandler(void) { static uint32_t last_sample_time = 0; if (EXTI_GetITS...

balkers by Associate II
  • 3050 Views
  • 5 replies
  • 0 kudos

2 x PWM with DMA

Posted on July 04, 2018 at 22:56I am doing now small project with STM32F0. I would like to generate two PWM signals simultaneously using DMA. Everything is working fine if I am starting one of two PWM Generators. When I start two works only first on...

slawek by Associate III
  • 2252 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.