2019-01-21 2:02 AM
How can i transmit data through usb fs without ftdi usb to uart converter?
2019-01-21 5:13 AM
Be a CDC/VCP Device? See USB Device/Host Examples in HAL trees
2019-01-23 2:51 AM
i use the cdc standalone i can send data to usart tx and measure the right output but how can i manage the same functions with my mcu like the ftdi pl2303A
2019-01-23 2:55 AM
Clive already said it - program STM32 to be a USB CDC/VCP device.
2019-01-23 2:58 AM
i programed it but the same thing which works for me with pl2303 ftdi( usb to uart port) is not working with my mcu via usart3
2019-01-23 3:40 AM
FTDI does not make Prolific parts.
Dont understand what "same function" is in this context. It is not going to act like a USART peripheral. You're going to want to manage the data into a buffer, and have routines to process and consume it from the buffer. Ie check a FIFO / ring buffer, not spin for RXNE
2019-01-23 8:20 AM
static int8_t CDC_Itf_Receive(uint8_t* Buf, uint32_t *Len)
{
HAL_UART_Transmit_DMA(&UartHandle, Buf, *Len);
//HAL_UART_Receive_DMA(&UartHandle,x Buf, *Len);
CDC_Transmit_FS(Buf, *Len);
return (USBD_OK);
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.