STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Output Two ADC Channels Over UART

I'm using the nucelo STM32F446RE dev board and attempting to output two ADC channels over UART (technically I think it's USART). I Can see in the debug tab that I'm reading the ADC channels correctly. I had been reading out one channel over UART 2 (t...

PAbdu by Associate II
  • 1966 Views
  • 2 replies
  • 0 kudos

How to create an fsdata.c file

trying to create a simple web page. I am using an fsdata.c file from one of the example projects and everything seems to be working. Now, I created a simple html file and need to convert it to an fsdata.c file. I have looked up this topic at vario...

IAgui by Associate III
  • 5363 Views
  • 7 replies
  • 5 kudos

STM32F7, QUADSPI and the data cache - odd behaviour

Posted on June 12, 2018 at 12:41Hi all,I have a board using the STM32F765, which uses the QSPI interface to fetch data from an FPGA. The normal sequence of operation is: A timer in the FPGA causes it to perform a sequence of events which produce a ...

andy by Associate III
  • 15502 Views
  • 32 replies
  • 0 kudos

STM32F4xx InputCapture and DMA

Posted on March 29, 2017 at 12:59MCU: STM32F446REBOARD: NUCLEO-64 STM32F446STM32 CUBEMX Version:4.20.0Library: STM43F4 1.15.0----------------------------------------------------------------------------------------------------------------------------...

0690X00000606eQQAQ.png
Zt Liu by Senior III
  • 3274 Views
  • 7 replies
  • 0 kudos

Resolved! 32F769-DISCO CubeMX 5.0.1 Ethernet Initialization hangs

Hello all,I built with CubeMX 5.0.1 a project from scratch using the default settings.The modifications:MMC --> SD (otherwise it wouldn't run. Probably ST will change it someday)LWIP enabled with fixed IP addressesAdded two lines to blink a LEDCompil...

Dangerous bug in cmsis_os Message implementation?

Posted on March 23, 2017 at 14:12I think that there is dangerous a bug in the cmsis_os implementation, because when you create a queue (thru osMessageCreate), it creates a queue in FreeRTOS with the item size based in the item size configured by the...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.