STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Jump from one Application to another STM32H743

Hi all,I have a problem when jumping from one application to another within my new STM32H7 system.Explaination: All my systems can be updated via my own bootloader (running on 0x800 0000) application, which communicates via USB port with a PC to my s...

GS1 by Senior III
  • 5367 Views
  • 10 replies
  • 0 kudos

Resolved! RM0395, STM32L412 and ADC12_CLK

Hello,RM0394 Rev. 4 chapter 16.4.2 clocks should note in a preamble or something similar that Dual clock and ADC12_CLK is not available on STM32L412. Reading through RM0394 I conclude that ADC clock is HCLK fixed on L412, but I don't see it stated ...

RM0394: Mismatch RM0394 and stm32l412xx.h

Hello,while RM0394 talks about CH18SEL and CH17SEL, in16.7.2 ADC common control register (ADC_CCR)stm32l412xx.h only knows ADC_CCR_TSEN and ADC_CCR_VBATEN .While the names in stm32l412xx.h are know to me from other devices, the names in RM0394 are ...

9 bit UART and DMA

Posted on September 18, 2017 at 07:46Hiya,I'm using the UART in 9 bit mode, with the 9th bit being used as an address indication.I have a version of this working well with 16 bit DMA transfers. Ideally though I want to use 8 bit DMA (byte wide) as a...

l m by Associate II
  • 5493 Views
  • 7 replies
  • 0 kudos

Problems with CAN on STM32F072RB

Hi, I'm trying to implement CAN on the STM32F072RB and I think I have added all the neccesary files. In stm32f0xx_hal_conf.h I have defined HAL_CAN_MODULE_ENABLED, but in stm32f0xx_hal_can.c it is not recognized. The question is that when compiling e...

pfc1 by Associate
  • 622 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.