STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L452RE in stop mode (both stop0 and stop2) sometimes decide to ignore EXTI interrupts for a second or so.

I run my CPU mostly (when possible) in stop2 mode. I want EXTI interrupt from few pins to wake it up.                                What i found is that sometimes it doesn't.                                                                           ...

WPuch by Associate II
  • 809 Views
  • 0 replies
  • 0 kudos

MDMA & internal FLASH R/W on STM32H7

Good morning,We're using an STM32H7 to acquire simoultaneously 3 ADC channels 16-bit @ 5MSPS, and we store data in an external eMMC. Everything worth seamlessly as follow : 3 slave-SPI with 3 DMA to internal flip/flop buffers ; MDMA to interleave dat...

A new learner wants to know

Hello everyone.İ am a new member.For several years i have been writing codes in pic ucontrollers as hobbiest. İ write codes in MPLAB X and CCS C for pic ucontrollers especially in 8 bit ones .But i want to turn my hobies into a job. When i see the jo...

omer_127 by Associate
  • 1612 Views
  • 3 replies
  • 0 kudos

STM32F103VCT TIM PWM Remapping problem

Dear guys.i have a problem.I used the STM32F103VCT.I control 3 color RGB LED using TIM1 PWM CH1~3 and i set the pwm parameter by CubeMX.After set the pwm, the pwm function is good work, but other device - USART1 is not work and debug mode is automati...

KLee.0 by Associate
  • 851 Views
  • 1 replies
  • 0 kudos

Pin configurations in low power modes

In the STM32L4 Nucleo examples, all GPIO on the processor are configured for analog mode before entering stop1 or stop2 modes. In a typical application, there will be some lines that must remain either high or low as to not turn on any external circu...

Resolved! STM32F0: Re-configure clocks after exiting stop mode

Hi All,I'm working with an STM32f091xC on a new design and I'm currently tryingto enable stop mode to conserve power without fully entering standbymode. I seem to be entering stop mode properly, but I'm having quite abit of trouble exiting stop mode....

RWebe.3 by Associate
  • 4003 Views
  • 2 replies
  • 0 kudos

What is the TIMx_CCy event?

ADC control register 2 (ADC_CR2)Bits 27:24 EXTSEL[3:0]: External event select for regular groupThese bits select the external event used to trigger the start of conversion of a regular group:0000: Timer 1 CC1 event0001: Timer 1 CC2 event0010: Timer 1...

YAn1 by Associate
  • 806 Views
  • 0 replies
  • 0 kudos

STM32F072RB systick not firing

I have an application running on an stm23F0-discovery the code is quite simple:HAL_Init();SystemClock_Config()while(1);The code is  built and debugged using IAR workbench 7.5The discovery clock config uses the internal HSI 8mHZ clock source. I have a...

Note to ST: HAL & STM32CubeMX are awesome!!!

Posted on September 18, 2017 at 19:27 To ST Microelectronics (especially the programmers who work on HAL & STM32CubeMX): I see a lot of bellyaching on these forums (especially from knowledgeable grizzled veterans) complaining about the HAL (Hardw...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.