STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SWO frequency?

In my debugger settings I got there is some SWO frequency difference means before 2 or 3 days its frequency value is 10Mhz but now it is only 2Mhz and from last days I have getting some errors. So plz tell me that such errors are coming due to this ...

LACTIC by Associate II
  • 5736 Views
  • 5 replies
  • 0 kudos

Resolved! What is the latest STM32F103RBT6 MCU revision available?

Hi everyone,I recently found myself having spent a lot of time working to get I2C to work on the STM32F103RBT6 (the problem: I2C begins life in the BUSY state).This is apparently due to an ADC noise problem, as described in this errata (p. 26):https:...

STM32 UART basic comunication

Hi,my first example for RS232 communication and my first problem.I have this output in the terminal:5 ''! Ëå˙˙˙ <00> 5 ''! Ëå˙˙˙ <00> 5 ''! Ëå˙˙˙ <00> 5 ''! Ëå˙˙˙ <00> 5 ''! Ëå˙ <00> 5 ''! Ë <00> 5 ''! Ëå˙˙˙ <00> 5 ''! Ëåë <00> 5 ''! Ëåë <00> 5 ''! ë...

JNova.0 by Associate III
  • 1493 Views
  • 2 replies
  • 0 kudos

STM32F769BI ADC_DMA interrupt causing debug stop

​​​​Hello, I am using the Stm32F769BI MCU.I am receiving 3 ADC channels through DMA.My problem is that debugging stops in the middle due to HAL_ADC_IRQHandler during debugging.To debug again, I must press the Run button again.I want to know why inter...

syoon.10 by Associate II
  • 2277 Views
  • 4 replies
  • 0 kudos

SPI: delay between write to TXDR and start of clock

Hello ,With SPI (SPI2 in my case) I experience a delay between a wite to TXDR and the start of the SCK activity in case of an empty TX fifo. It seems to be something like 5 SCK periods, so it changes with SCK frequency but this ratio remains. I check...

STM32L476 SPI half duplex receive clock

I configured the SPI2 port for bidirectional (BIDIMODE = 1) and rx (BIDIOE = 0), then enabled the port (SPE = 1). According to the RM the enable should immediately start sending clock pulses out the SCK pin and read data on the MOSI pin, since it is...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.