STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F746 QSPI: problem with Flash ROM(Winbond W25Q16JV)

I have a problem with QSPI. I try everything, but program doesn't work.I am using STM32F746 series MCU and I am trying to interface with a quad spi memory from Winbond (W25Q16JV).I am following the example found in this location:(I modified some inte...

KNono by Associate II
  • 7395 Views
  • 4 replies
  • 0 kudos

CAN bus does not work

Hello,I am using the STM32F7 in my project, which uses the CAN1. I create the project from cubemx and connect it to a STM32F4 evaluation board to test. I can see the Can signal via the oscillations cope after the transceiver, but no interrupt can be ...

kqian by Associate II
  • 2963 Views
  • 2 replies
  • 0 kudos

UART stm32F767ZI

Hello everybody,i wanted to send data from realterm serial to the stm32F767ZI but it dose not work. i cant see any message on my terminal. The same code is working good with STMF446re. The UART2 with STM32F4446re is connected to the USB Port. but wit...

Samuel1 by Associate III
  • 3249 Views
  • 3 replies
  • 0 kudos

STM32F£02R8 Clcok Issue

Hi All,So I have trying to get the UART to work for a while and after looking at the lines with scope, I discovered the the uart is twice the Baud rate I programmed it to and I don't know why.So I am running my uC of a 16MHz external crystal dividing...

glenn0010 by Associate III
  • 1732 Views
  • 3 replies
  • 0 kudos

H743 SPI slave receive not working in circular DMA mode

I try to make two H743 boards communicate each other. The master board sends a chunk (~300Bytes) unregularly and the slave board shall receive it and write it to memory via DMA. Interrupt mode working correctly.DMA Normal mode working correctly.DMA C...

CKosa by Associate II
  • 1504 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F429IGT6 was not working after a few cycles

When I upload my code the controller it was working fine for few cycles after that it gets stuck somewhere else and the code is not running. I checked it with the debugging mode in that when I run the code is working fine and when it gets struck I st...

AChan.15 by Associate II
  • 1846 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.