STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am having issues in reading the part of CCS811 from STM32L072xx. It is coming 0x80 instead of 0x81, how do I resolve it?

We are currently working on the interfacing of sensor CCS811 with STM32L072, and we are having trouble reading the Part ID of it. On reading register 0x20 the part id we are getting on serial monitor is 0x80 (While it should be 0x81). While checking ...

exit Standby mode delay with iwdg and rtc.

MCU: STM32H750exit Standby mode delay with iwdg and rtc.I find when I enable iwdg it seems will delay 1 second when exit standby mode. After trace code, I find it is hang in HAL_RTC_Init(),the RTC_EnterInitMode() will check weather the hrtc->Instance...

GChu by Associate
  • 1777 Views
  • 2 replies
  • 0 kudos

ADC in Low power run mode

Hi,I have configured ADC like  ADC_ChannelConfTypeDef sConfig;  /**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)   */ hadc.Instance = ADC1; hadc.Init.OversamplingMode = DISABLE; hadc.Init.ClockP...

Resolved! What books should I read to understand ARM MCU's?

Hi guys, I am in 12th grade and very interested in electronics. Ever since I knew about ARM microcontrollers (especially STM32 ARM MCU's) I've always wanted to build my projects using ARM MCU's, but I am unable to understand the technical information...

Sashvat by Associate II
  • 7227 Views
  • 18 replies
  • 0 kudos

SDRAM Extended Mode Register Write

I am using an STM32F769NI with a MT48H16M32LFB5-6 SDRAM chip, everything works fine. we are looking to set the drive strength to 1/4, 1/2 and full to evaluate the effect on EMC testing. From what I read in the programming manual, it states to perform...

0690X000008id91QAA.png 0690X000008id96QAA.png
gvigelet by Associate II
  • 642 Views
  • 0 replies
  • 0 kudos

How to properly configure the CAN2 RX Interrupt on STM32 ?

Hello,My RX0 Interrupt is not called and I don't understand why. If someone can help me, because I already tried lot of things.The problem is I never go in my "CAN2_RX0_IRQHandler()".I properly configured my CAN timings because the received frames ar...

ALuca by Associate II
  • 1017 Views
  • 0 replies
  • 0 kudos

STM32 I2C multi-device connection

Hello to everyone, I am a newbie on STM MCUs. I need to communicate 6 slaves and 1 master device. But I could not figure out. The master device has been selected Arduino mega due to some specifications. Slaves are responsible to drive motors, Arduino...

Sensortile standby high consumption

I am working on a project using the sensortile. When the MCU is not in use, it enters a standby mode. I measured a current of 4.5 mA in standby mode. What could be the cause of such a high consumption in standby mode?

RMous by Associate
  • 1589 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.