STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer Call back question ?

Dear Members,I have a callback :void Timer10_Callback() { seconds += 1;   if (seconds == 30) { minute = 1; seconds = 0; rpm=count; rps=(float)rpm/30; count=0; } }and main() inside while()current_rps = rps; i...

Activate LPUART1 on STM32L4 only when required

Hello, Please suggest a Software solution where I can power on the entire LPUART1 peripheral on STM32L4 only when I want. Any data received on the UART lines before I power on the LPUART1 must in no way be accessible to the MCU Hello,  I have an issu...

Grang by Associate
  • 822 Views
  • 0 replies
  • 0 kudos

STM32L073 adc polling async clock ?

hello, i am using the STM32L073 for adc reading. And want to use the async clocks for the dc voltage reading. so i dont need a high speed clock.The problem is when i tested the async clocks on adc , the measurement time was sometimes(30~40%) differen...

stress by Associate
  • 875 Views
  • 0 replies
  • 0 kudos

Zero crossing interrupt timer implementation

I am working on creating a reverse phase dimmer where the on/off timing for the 120/240 VAC sine wave is handled by an STM32L051C8Tx MCU. There is a separate analog circuit that generates a 3V3 pulse at every zero crossing and I take this as an input...

SPetr.6 by Associate III
  • 2384 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.