2019-07-01 3:51 AM
Hello,
My board includes SRAM, TFT (5.0 inch with ssd1963), NOR, NAND circuits.
When TFT is not connected, SRAM passes all tests (all memory read/write).
(I didn't test NOR or NAND)
if TFT is connected, Sram test fails any address. (Or TFT doesn't work properly in sram test)
(The project includes stemwin)
While writing/reading to sram, I think TFT too or the exact opposite.
Data , addresses, Read,write etc pins are common but all chip selects is following.
PG9 <-> FSMC_NE2 // NOR-CS
PG10 <-> FSMC_NE3 // SRAM-CS
PD7 <-> FSMC_NCE2 // NAND-CS
PG12 <-> FSMC_NE4 // TFT-CS
I wanted to ask that don't look hardware. in fact, I checked hardware before. All connections were OK. Isn't this state related CS? (by the way, there is not hardfault state)
how can such a situation occur?
Thanks.
2019-07-01 1:04 PM
i read the following article from a chinese source, ( between comments)
/*
* PG9 is connected to the CE side of NORFLASH in order to prevent the NORFLASH signal from affecting the SRAM.
* Here let CE = 1 first, that is, PG9 = 1, otherwise the SRAM will not test successfully.
* Or when the hardware is designed, the NORFLASH CE pin is pulled down.
*/
Why Sram and nor affect each other?
For PG9 is AF, if I don't write/read to NOR ( to only SRAM address), PG9 ( FSMC_NE2 - NOR_CS) can be enable?
PG9 <-> FSMC_NE2 // NOR-CS
PG10 <-> FSMC_NE3 // SRAM-CS
2019-07-01 1:27 PM
None of us here know what STM32 chip, board and source you are using.
2019-07-01 2:27 PM
You're right, Sorry,
Stm32F407ZET6, The connections is following,
TFT and SRAM are working alone but together, tft freezes (mcu is working) and sram test is getting faulty
TFT Connections:
PD14 <-> FSMC_D0 // DATA-0
PD15 <-> FSMC_D1 // DATA-1
PD0 <-> FSMC_D2 // DATA-2
PD1 <-> FSMC_D3 // DATA-3
PE7 <-> FSMC_D4 // DATA-4
PE8 <-> FSMC_D5 // DATA-5
PE9 <-> FSMC_D6 // DATA-6
PE10 <-> FSMC_D7 // DATA-7
PE11 <-> FSMC_D8 // DATA-8
PE12 <-> FSMC_D9 // DATA-9
PE13 <-> FSMC_D10 // DATA-10
PE14 <-> FSMC_D11 // DATA-11
PE15 <-> FSMC_D12 // DATA-12
PD8 <-> FSMC_D13 // DATA-13
PD9 <-> FSMC_D14 // DATA-14
PD10 <-> FSMC_D15 // DATA-15
// tft control pins
PF0 <-> FSMC_A0 // LCD-RS
PG12 <-> FSMC_NE4 // LCD-CS
PD4 <-> FSMC_NOE // LCD-OE
PD5 <-> FSMC_NWE // LCD-WE
K91G08U0B:
PD11 <-> FSMC_A16 // NAND-CLE
PD12 <-> FSMC_A17 // NAND-ALE
PD6 <-> FSMC_NWAI // NAND-RB
PD4 <-> FSMC_NOE // NAND-OE
PD7 <-> FSMC_NCE2 // NAND-CS
PD5 <-> FSMC_NWE // NAND-WE
SST39VF1601 :
PF0 <-> FSMC_A0 // NOR-ADDRESS-0
PF1 <-> FSMC_A1 // NOR-ADDRESS-1
PF2 <-> FSMC_A2 // NOR-ADDRESS-2
PF3 <-> FSMC_A3 // NOR-ADDRESS-3
PF4 <-> FSMC_A4 // NOR-ADDRESS-4
PF5 <-> FSMC_A5 // NOR-ADDRESS-5
PF12 <-> FSMC_A6 // NOR-ADDRESS-6
PF13 <-> FSMC_A7 // NOR-ADDRESS-7
PF14 <-> FSMC_A8 // NOR-ADDRESS-8
PF15 <-> FSMC_A9 // NOR-ADDRESS-9
PG0 <-> FSMC_A10 // NOR-ADDRESS-10
PG1 <-> FSMC_A11 // NOR-ADDRESS-11
PG2 <-> FSMC_A12 // NOR-ADDRESS-12
PG3 <-> FSMC_A13 // NOR-ADDRESS-13
PG4 <-> FSMC_A14 // NOR-ADDRESS-14
PG5 <-> FSMC_A15 // NOR-ADDRESS-15
PD11 <-> FSMC_A16 // NOR-ADDRESS-16
PD12 <-> FSMC_A17 // NOR-ADDRESS-17
PD13 <-> FSMC_A18 // NOR-ADDRESS-18
PE3 <-> FSMC_A19 // NOR-ADDRESS-19
PE4 <-> FSMC_A20 // NOR-ADDRESS-20
PE5 <-> FSMC_A21 // NOR-ADDRESS-21
PE6 <-> FSMC_A22 // NOR-ADDRESS-22
PG9 <-> FSMC_NE2 // NOR-CS
IS61WV51216EDALL:
PG10 <-> FSMC_NE3 // SRAM-CS
PE0 <-> FSMC_NBL0 // SRAM-LB
PE1 <-> FSMC_NBL1 // SRAM-UB
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.