STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What timers are free

Cube/HAL shows some nice Timers, are they free. That is are they used by for instance HAL_Delay or something else. What about the examples and their timer usage.

LMI2 by Lead
  • 2037 Views
  • 3 replies
  • 0 kudos

BUG in bxCAN HAL

I'm usingSTM32Cube FW_F7 V1.15.0There is a bug in stm32f7xx_hal_msp.c which prevents reinitialization of CAN1void HAL_CAN_MspInit(CAN_HandleTypeDef* hcan) {....  HAL_RCC_CAN1_CLK_ENABLED++;  if(HAL_RCC_CAN1_CLK_ENABLED==1){   __HAL_RCC_CAN1_CLK_ENABL...

AT by Associate
  • 1096 Views
  • 1 replies
  • 0 kudos

STM32L4 not exiting sleep mode

When trying to implement sleep mode it appears the code enters and exits sleep mode once and then gets stuck in sleep mode after and will not wake back up. I posted some code below of what I believe affects the sleep function. I want the code to slee...

JDarg by Associate II
  • 855 Views
  • 0 replies
  • 0 kudos

STM32L412 "Reference voltage buffered output" feature

Hello,DS12469 Rev 6 in Features on page 1 lists "Accurate 2.5 V or 2.048 V reference voltage buffered output" under  "Rich analog peripherals". However "Table 2. STM32L412xx family device features and peripheral counts (continued)" says "Internal vol...

How to make partition binaries for STM32F103ZC using Makefiles

I just switched from Arduino to the ST HAL library, I'm quite new to both the structure and makefiles in general. I'm using a chip that allows for multiple parts that can be used for OTA's for example. While I have made a working project that can upl...

JGale by Associate II
  • 810 Views
  • 0 replies
  • 0 kudos

two kinds of deadtime config

yes , above fig about two kinds of config deadtime ,I don't know how to get that waveformI have readed RM about deadtime chapter,but I still not clear

0690X000009Yr8aQAC.png

Why SDADC could't not start

Hi everyone,I designed my custom board with stm32f373c8. SDADC runs properly when voltage reference is setted with Vref or VDDA. But when voltage reference is setted with internal 1.8 volt or internal 1.2 , sdadc could't start. It waited while loop t...

Sy??n by Associate
  • 911 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.