STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 Timer Output Compare mode (OC mode)

hi sir, I want to use timer channels to OC mode. In that same timer interval i need set time to channel 1 come 1 time and channel 2 comes 5 times.example: In 1 milli second timer i need set & reset channel 1 for time and every 200 micro second set ...

srikanth by Associate III
  • 3483 Views
  • 4 replies
  • 0 kudos

Resolved! BSDL file for STM32L4R5ZIT6

I am trying to run a boundary scan test on a custom board with a STM32L4R5ZIT6, My boundary scan tool of choice has highlighted some inconsistencies with the pins. When I set certain pins the wrong pins get set.I checked the resources section on you...

Rclar.13 by Associate II
  • 2559 Views
  • 2 replies
  • 0 kudos

I'm trying to port some firmware from nucleo-F334 to nucleo-G474 for the HRTIM timers and the CubeMX for G474 for HRTIM1 is not working. I found some missing statement in the initialization.

I found that the CubeMX 5.3 initlization code missing a part; specifically the HRTIM clock initialization where the PLL is defined. There's a related constant that also needs to be defined. In any case can someone confirm the problem and how long it ...

WTom by Associate III
  • 890 Views
  • 0 replies
  • 0 kudos

Resolved! Problem with timer and input capture, timer does not run

Does anyone have experience with getting the timer to run with input capture, I am unable to make the input capture function.I have a working system with STM32F03 (M0) devices initialization generated by CubeMX. Now I am testing an identical system w...

TMalt by Associate II
  • 3505 Views
  • 4 replies
  • 0 kudos

HardFault on STM32F765

Hi,My code is generating a HardFault condition, is not every single time it pass the main loop, but after the first 5s it stops.The Hardfault not happen every time in the same line, that is what have been so difficult to track down, but it always sto...

0690X000009YoaXQAS.png 0690X000009YoamQAC.png

ADC channel 0 with DMA ?

Dear Members,I tried to initialize ADC1 channel 0 with DMA but I got not output yet,Init code :ADC_HandleTypeDef hadc; DMA_HandleTypeDef hdma_adc;   /* ADC init function */ void MX_ADC_Init(void) { ADC_ChannelConfTypeDef sConfig = {0};   /**Confi...

Disabling Hex File Generation?

Setting up an embedded project with the Blinky Hello World project, and my build keeps making a .hex file when I don't really want it to. There isn't anything in the pre or post build steps that should be generating a .hex file (the way I found onli...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.