STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! can I use all 8 UARTs of STM32F091VC?

Hi All,Currently, I'm working on project wherein I need the maximum number of UARTs I can get. After doing some research, I came across the STM32F091VC controller which has the 8 UART (max number of UARTs ST can provide). Unfortunately, there is not ...

Please Help - Timer not generating output on pin

I'm attempting to output a 50% duty cycle clock signal on Port C bit 7.I running on a STM32F407I have verified that that output is working when set the pin as function 0 and toggled.Using function 2 when associated with the timer 3 channel 2I have al...

Joe.H by Senior
  • 1148 Views
  • 2 replies
  • 0 kudos

Accurately measuring board current consumption.

Hi, I'm trying to get as accurate a power measurement as possible on an NUCLEO-F103RB board. I set it up using STM-CUBE to run at 1MHz and all peripherals in the default state. The only code I am running (once initialization is complete) is an empty ...

Filtering ADC output with FIR ?

Dear Members,Dear Members,I got a FIR filter coefficient from matlab :/* General type conversion for MATLAB generated C-code */ #include "tmwtypes.h" /* * Expected path to tmwtypes.h * C:\Program Files\MATLAB\R2018b\extern\include\tmwtypes.h *...

BlueNRG-2 IIC error with reading more than 16 bytes

Hi, I am working on BlueNRG-2 and I need drive NFC-EERPOM(M24SR64). I tried to read from M24SR64, I got error when the reading bytes were more than 16.(It was ok <= 16 bytes), it stuck on the while loop as below. I put my readfunction and init func...

SZhan.5 by Associate
  • 1559 Views
  • 2 replies
  • 0 kudos

Get STM32F4 Software

Can you please help me to get quick link to download STM32479I-EVAL demonstration software? I can see related resources but unable to find the demonstration software.

TJagd by Associate
  • 996 Views
  • 1 replies
  • 0 kudos

STM32F4. Interrupt from DMA burst writing only once appears

MCU is STM32F405. I write data array to output pins using DMA mem to peripheral (DM2 stream6 channel0). Trigger is TIM1 CC1 event. Also I use DMA2 stream5 channel6 for write to TIM1 registers. Trigger is TIM1 UEV event. So the writing and interrupt D...

Alex Mach by Associate III
  • 3837 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.