STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L073 : Power on reset

I just saw Power on reset feature in Pic (https://microchipdeveloper.com/8bit:por). It can hold mcu a little bit until the power is stable, before starting the hardware initialization. I would like to know if this feature is avalilable on stm32.I ha...

SRodb by Associate
  • 1360 Views
  • 1 replies
  • 1 kudos

Resolved! H743 using RAM_D1 can not handle std:string greater than 15

HelloI've been working on a project on an nucleo F411RE and everythings been going fine.I then had to port the project to nucleo H743ZI.As i am using the DMA i had to change the ram from DTCRAM to RAM_D1.Before the change to RAM_D1 i could have strin...

NMunt by Associate II
  • 4939 Views
  • 9 replies
  • 0 kudos

STMPE811 touch controller Interfacing with STM32F746BGT6

We are developing the TouchGFX project in  STM32F746BGT6 and using resistive TouchscreenWe have created the project using ST CUBEMX for discovery board .the same project code has been used for our customized PCB.For this we need to interface the STMP...

STM-User by Associate II
  • 963 Views
  • 0 replies
  • 0 kudos

Hard reset Interrupt issue in STM32F103RB

I am testing EXTI interrupts on STM32F103 board. The device works properly when soft reset is given. Interrupts are triggered properly. But when I give hard rest to the device(Like power off & power on) , it fails to initialize STM32. Maybe it gets a...

sne_123 by Associate III
  • 919 Views
  • 0 replies
  • 0 kudos

Resolved! How do the GPIOs actually work?

That question started bothering me when I was struggling with TLE493D that started interrupting using the i2c clock line.It looked like the i2c in the F429 was gone bananas and keeping the i2c stuck (busy).I was thinking of feeding the i2c the clock ...

STM32F103RCT6 I2C SLAVE transmitter CAN NOT GENERATE ACK

Currently I try use STM32F103RCT to implement I2C slave to communicate with master. When master sent address with write bit , there is no any problem and all data can be transmitted to slave through I2C, but when master try to read, it seems big prob...

Liu0155 by Associate II
  • 1069 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.