STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Does the HRTIM support a DMA-based input capture (IC) mode?

I would like capture the CNT register and transfer it to a circular buffer on every rising/falling edge on 10 different signal lines. Is this possible and is there a reference which describes how to do this?This is on the STM32H7 series.I have read ...

TDK by Super User
  • 3103 Views
  • 5 replies
  • 2 kudos

Resolved! STM32L4R5ZI using OCTO-SPI without flash memory?

Hi,I'm using a STM32L4R5ZI and i want to use OCTO-SPI with my own hardware. My question is, can i use the OCTO-SPI without a external flash memory to communicate from the MCU to the PC ? Up to now i tried the provided OCTO-SPI example provided by STM...

what is the source of clock for CANBUS

Hi,what is the clock source for CANBUS in STM32F767?I have referred the manual ,but still i cannot get the clear answer from it.the main reason to know the clock source is to calculate the bit timing .ThanksVimal

VPras by Associate II
  • 1383 Views
  • 2 replies
  • 0 kudos

Resolved! How can I prevent the I2C from getting interrupted?

There's a sensor applied to the I2C as a slave. Also on this microcontroller there's a communication running on the UART-Interface in blocking mode. If the UART has to transmit a huge amount of data, it seems that the I2C (also blocking mode) can get...

stm32f103rbt6 i2c1 remap not working

i am using stm32f103rb i think i have found a bug i am trying to use i2c1 on pin port b 8 and 9 for that you have to remap i2c1 in afio mapr register i have done that but in debug session i note that the bit never get set i have attached code and deb...

Iyar.388 by Associate
  • 1354 Views
  • 1 replies
  • 0 kudos

Debug Cortex-M error

Hi,I want to debug a code for USART ISR Handler. The code is working fine. But If I debug, I am getting this error. I am using keil uvision.Cannot access target. shutting down debugging session.Why this error is coming. And how to over come this? I a...

Kumar B by Associate II
  • 3168 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.