STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TIM1 ch1 as pwm, ch2 as cc to trigger adc caputre

On STM32F105 chip, i need to output a pwm, then adc caputure the voltage on pwm high stable level.So i try to set tim1 ch1 to pwm out, and then set tim1 ch2 as compare output wih no pwm to trigger adc capture with DMA. (CC2<CC1)Eventrually, i cannot ...

Usart as SPI

Are there any example that uses USART as SPI ? Currently I am using stm32g071kbt6 mcu for a project and i have to use USART peripheral as SPI. Other SPI peripherals on use. I found a few presentation about USART that says USART can be use as SPI and ...

Emin ATES by Associate II
  • 2085 Views
  • 4 replies
  • 0 kudos

Peripheral sharing with dual core H7

I am working with a dual core processor for the first time & am wondering if i need to use a semaphore to block one processor while the other reads a peripheral register?In my application the M4 is being used as a slave for some concurrent processing...

RMcCa by Senior II
  • 2271 Views
  • 6 replies
  • 0 kudos

Resolved! How can i make a camera with stm32f4disc?

​Hello,  I have stm32f4disc and baseboard, ov 9655 camera module, l​cd screen. ​ I want to make a camera. Who has guides or tutorials that can help me. Thanks​

MHMallek by Associate II
  • 1045 Views
  • 1 replies
  • 0 kudos

DMA for loading PWM values directly

I am attempting to use the DMA to auto-load PWM values for a motor control application. An example very similar to what I want to do is given in the RM0090, section 17.4.20 (for STM32F427). However, I'm missing some detail and can't get the DMA to tr...

STM32F030C8 not entering Read Memory Level 1

STM32F030C8 - I'm not using any of the ST libraries.I'm attempting to secure the mcu.I unlock flash and unlock the option write - verified.I am using a J-Link debugger to verify the process.Option byte before process == 0xaa55 - or level 0 accessI er...

Joe.H by Senior
  • 950 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.