STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi, I'm using the MCU STM32l476, and I have a problem with RTC. The RTC works only if the board is turned on. When the board is turned off or it's sent a command to the MCU go to shutdown mode, the RTC is reset to zero values.

According to the datasheet, there is shutdown mode with and without RTC, so I believe it's a problem of configuration. Can be some parameter of configuration that is missing? How to configure the shutdown mode with RTC?Thanks!

FDigi by Associate III
  • 4358 Views
  • 12 replies
  • 0 kudos

I use stm32 eclipse to add two folders in a folder named drivers. One is for my .c files named src and the second is inc for my header files. The .c can not seem to read the header files when called up on.

I use stm32 eclipse to add two folders in a folder named drivers.  One is for my .c files named src and the second is inc for my header files.  The .c can not seem to read the header files when called up on.  I am new to this so the answer should be ...

UART IDLE LINE interrupt

hi, I need some advice, I'm trying to implement the IDLE_LINE interrupt for a UART with DMA. I simply need to receive a variable length buffer. I searched the internet and put together various code snippets, I came to this:in main.c:__HAL_UART_ENABLE...

Reading RTC after wakeup from standby mode

Good day,I'm using an STM32L152RE and utilize the standby mode quite often. Upon cold start, I set the RTC and I am able to enter standby mode and wakeup from standby mode based on the RTC time and alarm events.My problem is this: I don't understand ...

Resolved! STM32CubeProgrammer in Linux

Posted on February 22, 2018 at 21:09I have just installed the new STM32CubeProgrammer for Linux but it won't run. I see the error 'Error: Could not find or load main class com.st.app.Main'. Anyone else come across this problem that has a fix?I went ...

Does any one have an example for dual can stm32f407?

Hello. I'm newbie in stm32 family, so I need in high speed bus 500 kbs catch one packet with standart id and change tree bytes. If somebody have an example fow my procesoor dual can, please give it for me. I need trancieve from can1 to can2 all packe...

Resolved! CAN Bus Extid paramater is not transmitting

Hello, I have setup the CAN bus to transmit and has been working fine. I now need a feature which requires the ExtID but this isn't getting transmitted. I have debugged both and can see that the ExtId is getting transmitted but not received, I'm wond...

0690X00000ArnH2QAJ.png 0690X00000ArnGdQAJ.png
MikeP by Senior
  • 3882 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.