STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f7 uart rx interrupt mode running only once

Hi,we have custom stm32f7 board with debugger connected and we are configuring UART RX in interrupt mode. In main function code is like below and uart rx interrupt is working fine for only once.uint8_t aRxBuffer[15];if(HAL_UART_Receive_IT(&UartHandle...

Tp by Associate II
  • 889 Views
  • 0 replies
  • 0 kudos

STM32F103RCT6 UART5 not working

Hi all,I'm using uart5 of stm32f03rct6 with Std lib but it's not working. However, when i use cubemx with HAL, It works perfectly. Anyone can help me check my code :( USART_InitTypeDef USART_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; GPIO_In...

According to IPC-A-610 revision G, you can have a 30% void in your BGA device. I every pin in the STM32F417IGH6 device was missing 30% of its connection, would the device still work per the datasheet?

IPC-A-610 revision G page 8-93 indicates that you can have a 30% void in your solder ball. We recently had a STM32F417IGH6 device over heat. Upon X-ray, we discovered that about 80% of the solder balls had voids near 30%.

OPAMP4 Mode StandAlone with DAC_OUT1_INP (STM32F303CCT6)

Hiall,Working with the OpAmp4, in the CubeIDE, it seems like it is poossible to connect the DAC_OUT1 to INP, internally. I tested in some ways, and its appears the signal form DAC_OUT1 dont reach INP of the OpAmp.Reading the RM0316, page 112, the tab...

JAlca by Senior
  • 707 Views
  • 0 replies
  • 0 kudos

MBEDTLS HANDSHAKE_FAILURE on STM3210C board

Hi, I’m trying to establish TLS communication with my local mosquitto broker.The handshake always fails, the broker does not accept the hello client and I cannot understand why …Below the decoded messages that pass over the network.Messages are captu...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.