STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I'm monitorating heart rate by the MAX30100(https://img.filipeflop.com/files/download/Datasheet_MAX30100.pdf) using the MCU STM32F4. I'm trying read the IR and RED data from the FIFO, but all returns are **ZERO**.

I'm monitorating heart rate by the MAX30100(https://img.filipeflop.com/files/download/Datasheet_MAX30100.pdf) using the MCU STM32F4. I'm trying read the IR and RED data from the FIFO, but all returns are **ZERO**. The method `MAX30100_Get_Num_Samples...

I am developing a product that uses an STM32F103. I spent the last two days debugging the USART1 port due to multiple issues with the controlling SBC and the ARM GNU stdio lib.

I got everything working but it turns out that there is an undocumented feature with the RTS line. Even after I bypassed the HW bug with the CAN peripheral (that was documented in your errata sheet), it still would not raise the RTS line when its RD...

PhilSter by Associate II
  • 1778 Views
  • 4 replies
  • 0 kudos

Resolved! Is a single FSMC access interruptable ?

Hi,I'm wondering if a FSMC access interruptable? in another word, do I have to disable interrupt before accessing to the external memory with FSMC, then recover the interrupt status after? Or just use it as it is a internal memory, access it freely? ...

STM32H743 cannot use HAL_SPI_Transmit_DMA with Nor Flash

I'm working on STM32H743 applied SPI DMA with MT25 QL128ABA1(NOR Flash) and initial mode to master mode.My problem is I cannot receive (HAL_SPI_Receive_DMA) return data when I use HAL_SPI_Transmit_DMA by run code through but I can receive return data...

0690X00000AsLVSQA3.png
ryawi by Associate
  • 803 Views
  • 0 replies
  • 0 kudos

Where do I read OCxREF?

I need to set up a PWM without an output pin but be able to read the state of the "virtual" signal. In the reference manual this state is referred to as OCxREF (OC1REF, OC2REF etc.). However, I'm clearly going senile as I can't find this in any of th...

PMath.4 by Senior III
  • 2019 Views
  • 3 replies
  • 0 kudos

STM32L151RCT6 PC3 5V Tolerant GPIO

HiIn the STM32L151RCT6 Datasheet (August 2017, DocID022799 Rev 13) it is specified that the PC0 to PC10 GPIO pins are 5V tolerant except the PC3, that should have a standard 3V3 IO structure. We have measured these GPIOs and have found that the PC3 h...

How to use the "errno" in STM32F103CBT6?

Hello!I'm using some of the string conversion functions, who's declarations are present in the "stdint.h" file. at present I'm using "strtol" and "strtod". According to the library "the value of the macro ERANGE is stored in errno, If the correct val...

ULPI clock noise + I/O compensation cell

We are seeing around 400mV of ULPI clock noise (60MHz) on the remaining DAC output with an STM32F427. The data sheet suggests to use the I/O compensation cell when using 100MHz outputs (like all the ULPI interface signals), but information about how ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.