STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STLINK-V3MINIE connecting SWO and VCP_TX pins

I am making an adapter between 6‐pin target debug header and 14-pin STDC14 connector. The same cable will be used to program and debug both M0+ and M4 targets.Can I hard-wire SWO (pin 8 ) and T_VCP_TX (pin 14) together? The idea is to have an option ...

maple by Associate II
  • 1187 Views
  • 2 replies
  • 0 kudos

Connectivity setup for SDMMC1 in STM32 Cube IDE

 I am working on interfacing MicroSD card with STM32H757I-EVAL. I am following the same steps to setup and configure SDMMC1, as mentioned in this video https://www.youtube.com/watch?v=-0kFwp0ao6k  @2:56 but there is DMA setting option under SDMMC1 co...

priya_12 by Associate II
  • 898 Views
  • 1 replies
  • 0 kudos

Resolved! HRTIM Triggering ADC

Hi,I am currently working with the STM32F334 and STM32G474 microcontrollers, and I have a couple of technical questions that require deeper insight into how the HRTIM (High-Resolution Timer) operates in these devices.Q1. Can HRTIM generate a high-res...

s2000 by Associate
  • 2209 Views
  • 3 replies
  • 2 kudos

Resolved! CAN FIFO filling faster than flushing

We set up classic CAN on the stm32h747I-DISCO dev board and listen for interrupts on every message:extern "C" void HAL_FDCAN_RxFifo0Callback(fdcan_handle* hfdcan, std::uint32_t RxFifo0ITs) { if ((RxFifo0ITs & FDCAN_IT_RX_FIFO0_FULL) != RESET) ...

chipchop by Associate II
  • 2274 Views
  • 4 replies
  • 2 kudos

FMPI2C DMA Not working - STM32F446

Hello All, I am trying to talk to an FRAM over FMPI2C on the STM32F446 using DMA, but the DMA is not able to "start". I am using the Mem_Write_DMA function in stm32f4xx_hal_fmpi2c.c.When I do a side by side comparison with the Mem_Write_DMA function ...

reserving high-cycle flash

What's the difference between enabling high cycle flash from option bytes on an H5 versus just using that section of flash by reserving it in the linker instead, apart from the ECC change?

debug and code non corresponding

I have an application that debugs correctly when I loads it at address 0x08000000.I'd like to use a bootloader, so I've changed the ld file, and choose, as flash origin, the address FLASH (rx) : ORIGIN = 0x08020000, LENGTH = 1920KBut, in this case, w...

IVent.1 by Senior
  • 1213 Views
  • 2 replies
  • 0 kudos

Resolved! STM32U5A5 Hard fault setting SYSCLK > 64Mhz

I'm trying to crank up the clock to Timer1 to be able to count high frequency events with better resolution.  If I set the SYSCLK to 128 I get a hard fault when my code reaches SystemClock_Config().  Even if I keep the AHB bus at the same speed (64Mh...

moylando_0-1747000454293.png moylando_1-1747000500208.png
moylando by Associate III
  • 6432 Views
  • 19 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.