STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Regarding SPI DMA Rx issue when using SPI 8 bit mode

Hello,I have had an issue with SPI Rx DMA. In short, I recieve twice as many bytes as I expect when using SPI 8 bit mode (STM32CubeIDE setting), but not in 16 bit mode.A brief description of the project:Im using an external accelerometer with 220ksps...

AAnn? by Associate
  • 969 Views
  • 1 replies
  • 0 kudos

Is STM32H743ZIT6 multicore or not

When I read the datasheet, the introduction doesn't mention the number number of cores. Digikey says this is a multicore chip. Mouser doesn't either talk about multicore.Several pages down (14) on the datasheet I can read that this is indeed a multic...

LMI2 by Lead
  • 2138 Views
  • 5 replies
  • 0 kudos

STM32F446ZE doesn't enter in Standby mode

Hi,I am using Standby mode on STM32F446ZE, but I faced with a problem. Sometimes MCU doesn't enter in this mode. Exiting Standby mode via RTC wakeup.Below is present steps which I perform for entering StandbySCB->SCR |= 0x00000004;PWR->CR |= 0x000000...

Resolved! PWM capture using Rising, falling EXTI

Hi all,I am capturing 10 pwm pulses from proximity sensors by making the all pwm pins in rising falling interrupt mode.PWM is captured by a timer at every 100us interrupt.some times pulses are missing, I don't know why this is happening.I am sharing ...

gladdy by Associate II
  • 4935 Views
  • 10 replies
  • 0 kudos

How to use Rotary Encoder effectively in external interrupt

Hi there this is Akash, I am doing a project on STM32F100RB Discovery Kit, in this project I am controlling stepper motor with some parameter given by the user using rotary encoder, basically I want to run the motor in the while loop, and through ext...

Akash R by Associate II
  • 2699 Views
  • 4 replies
  • 0 kudos

Is there a limit on how many bytes to send over I2C from the slave? The MCU is STM32F469NI, and I have programed the board to act as an slave, it works fine if amount of data sent from slave is less than 100 bytes, but data gets corrupted if sent more.

Is there a limit on how many bytes to send over I2C from the slave?The MCU in question is STM32F469NI, and I have programed the board to act as an slave using HAL, it works fine if amount of data sent from slave is less than 100, but gets corrupted f...

fzx by Associate II
  • 3930 Views
  • 4 replies
  • 0 kudos

Programing STM32F030 faild: No device at targed

Hi, I designed my first own board with a STM32F030F4P6 on it. Additionally a got me a ST-Link V2 for programing and debugging. As IDEIuse CubeMXIDE. I already successfully programed some Nucleos with it. With my own board I don't get a connection to ...

Mister232 by Associate II
  • 2715 Views
  • 3 replies
  • 0 kudos

STM32H7 lowest possible standby current, any examples?

HI!I am currently trying to minimise the standby consumption of a STM32H7 down to theabsolute minimum. Only the change of one Pin (PA0) is selected as wakeup event. No need for backup ram, Pin drivers, RTC nor anything else. The MCU shall only switch...

Microman by Associate III
  • 1466 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.