STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FLASH DATA WRITE PROBLEM IN STM32H743IIK6

Hello i want to write some variable data on internal flash using HAL library but it not writing.I am using blow code to write data to flash.can you please tell what am i doing wrong.#define FLASH_ADDRS   0x081E002A#define FLASH_DATA_W...

RShar.9 by Senior
  • 1579 Views
  • 3 replies
  • 0 kudos

QUADSPI + DMA, reading too many bytes?

Hello, so I am trying to write a driver for a GigaDevice GD5F2GQ4xFxxG part, that uses the QUADSPI peripheral. So far so good, but seeing some unexpected results and when I dug into it, I think I observe that a read command is acquiring more bytes t...

STM32F407G-DISC1 for Window 10

Hi, As per product data sheet, STM32F407G-DISC1 discovery board is compatible with Windows® OS (XP, 7, 8). But I have window 10.Does this discovery board supports window 10?Thanks and Regards,Shailesh Kumar

SKuma.71 by Associate
  • 1442 Views
  • 2 replies
  • 0 kudos

STM32F303 ADC Sequence Conversion Problem

Hello I am trying to use STM32F303VCT6 ADC1 to measure 4 channels in sequence. I am using TIMER 3 to trigger start of sequence conversion. I am using DMA1 to transfer data to an array. My code is as follows:ADC Configuration:ADC_InitTypeDef ADC...

MAbba.8 by Associate II
  • 792 Views
  • 0 replies
  • 0 kudos

Print to Serial port of an STM32F030F4P6

Hi.I have a diy board with STM32F030F4P6 Atollic TrueSTUDIO 9.3.0 and STM32CubeMX 5.2.1.I want to use it 's serial port in order to print (for debugging), like in Arduino we use the Serial.print().I 've followed a few things I found on the internet b...

openOCD by STM

Hello,Is there a version of openOCD compiled by STM which contains all the latest cards (notably the NUCLEO-G071RB) and is it possible to obtain the command generated by STM32CubeIDE configured with openOCD.Because I would like to use another IDE (CL...

ADEVL.1 by Associate II
  • 12322 Views
  • 17 replies
  • 0 kudos

Resolved! Openocd not working with STM32F750

I was successfully using openocd with GDB with STM32F746-DISCO. However, my new STM32F750-DISCO does not work.I use this commands:openocd -f /usr/share/openocd/scripts/board/stm32f7discovery.cfg telnet localhost 4444 reset halt flash write_image eras...

KMaen by Associate III
  • 1447 Views
  • 1 replies
  • 0 kudos

Can the ADC operation frequency be more than 60Mhz?

According to the spec, it says the ADC clock frequency is up to 60Mhz for a single channel. Does it mean we cannot apply the ADC clock more than 60Mhz to the ADC modules? But in the STM32Cube example code, the ADC clock applied to the ADC module is ...

0690X00000Bw7NHQAZ.jpg
LHsu.1 by Associate
  • 2906 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.