2020-01-17 10:00 PM
Hello I am trying to use STM32F303VCT6 ADC1 to measure 4 channels in sequence. I am using TIMER 3 to trigger start of sequence conversion. I am using DMA1 to transfer data to an array. My code is as follows:
ADC Configuration:
ADC_InitTypeDef ADC_InitStructure;
ADC_CommonInitTypeDef ADC_CommonInitStructure;
/* Configure the ADC clock */
RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div16);
/* Enable ADC1 clock */
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_ADC12, ENABLE);
ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;
ADC_CommonInitStructure.ADC_Clock = ADC_Clock_AsynClkMode;
ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_1 ;
ADC_CommonInitStructure.ADC_DMAMode = ADC_DMAMode_Circular;
ADC_CommonInitStructure.ADC_TwoSamplingDelay = 0;
ADC_CommonInit(ADC1, &ADC_CommonInitStructure);
ADC_InitStructure.ADC_ContinuousConvMode = ADC_ContinuousConvMode_Disable;
ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;
ADC_InitStructure.ADC_ExternalTrigConvEvent = ADC_ExternalTrigConvEvent_4; /*TIMER
3 Triggers ADC*/
ADC_InitStructure.ADC_ExternalTrigEventEdge = ADC_ExternalTrigEventEdge_RisingEdge;
ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;
ADC_InitStructure.ADC_OverrunMode = ADC_OverrunMode_Disable;
ADC_InitStructure.ADC_AutoInjMode = ADC_AutoInjec_Disable;
ADC_InitStructure.ADC_NbrOfRegChannel = 4;
ADC_Init(ADC1, &ADC_InitStructure);
/* ADC1 regular channel1 configuration */
ADC_RegularChannelConfig(ADC1, ADC_Channel_1, 1, ADC_SampleTime_1Cycles5);
/* ADC1 regular channel2 configuration */
ADC_RegularChannelConfig(ADC1, ADC_Channel_2, 2, ADC_SampleTime_1Cycles5);
/* ADC1 regular channel3 configuration */
ADC_RegularChannelConfig(ADC1, ADC_Channel_3, 3, ADC_SampleTime_1Cycles5);
/* ADC1 regular channel4 configuration */
ADC_RegularChannelConfig(ADC1, ADC_Channel_4, 4, ADC_SampleTime_1Cycles5);
ADC_RegularChannelSequencerLengthConfig (ADC1, 4);
/* Configure ADC Channels 1,2,3,4 as analog input */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;
GPIO_Init(GPIOA, &GPIO_InitStructure);
/* Calibration procedure */
ADC_VoltageRegulatorCmd(ADC1, ENABLE);
/* Insert delay equal to 5 ms */
Delay(5);
ADC_SelectCalibrationMode(ADC1, ADC_CalibrationMode_Single);
ADC_StartCalibration(ADC1);
while(ADC_GetCalibrationStatus(ADC1) != RESET );
ADC_DMAConfig(ADC1, ADC_DMAMode_Circular);
ADC_DMACmd(ADC1, ENABLE);
/* Enable ADC1 */
ADC_Cmd(ADC1, ENABLE);DMA1 Configuration:
DMA_InitTypeDef DMA_InitStructure;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_DMA1, ENABLE);
DMA_InitStructure.DMA_M2M = DMA_M2M_Disable;
DMA_InitStructure.DMA_MemoryBaseAddr = (uint32_t)&adc_values; /*Array to hold ADC
values*/
DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralSRC;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_High;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
DMA_InitStructure.DMA_BufferSize = 4; // in data unit
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR;
DMA_Init(DMA1_Channel1, &DMA_InitStructure);
DMA_Cmd(DMA1_Channel1, ENABLE);TIMER 3 Configuration:
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
/* TIM3 Periph clock enable */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE);
/* Time base configuration */
TIM_TimeBaseStructInit(&TIM_TimeBaseStructure);
TIM_TimeBaseStructure.TIM_Period = 0x2328;
TIM_TimeBaseStructure.TIM_Prescaler = 0x0;
TIM_TimeBaseStructure.TIM_ClockDivision = 0x0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure);
/* TIM3 TRGO selection */
TIM_SelectOutputTrigger(TIM3, TIM_TRGOSource_Update);
/* TIM3 enable counter */
TIM_Cmd(TIM3, ENABLE);In main I have used following code to start the ADC process:
DMA_Config();
ADC_Config();
TIM_Config();
/* wait for ADRDY */
while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_RDY));
/* Start ADC1 Software Conversion */
ADC_StartConversion(ADC1);The problem I am facing is that my code can only convert the channel which is highest in the sequence. For example, for the configuration given above, I am able to see correct conversion value only on channel 1 of ADC 1, because its rank is 1 in the sequence. I have tried changing the channels in the sequence to confirm that the channel with highest rank i.e. first channel in sequence gets converted. I have not enabled any interrupts.
Kindly see the code and tell me what I am missing.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.