STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm uart communication voltage

I want to use stm32f407gt with nextion touch screen. Display and stm will connect via to uart(Rx Tx pins). Stm work with 3.3V and nextion works with 5V. It will effect to communication ?

IDANI.1 by Associate
  • 3258 Views
  • 1 replies
  • 0 kudos

STM32F439 SDMMC Command Timeout

Hello all,I access SDMMC directly through the APIs: HAL_MMC_WriteBlocks() and HAL_MMC_ReadBlocks().Sometimes the access to SDMMC does not does not succeed with Timeout error.Can you please advise me?Thanks in advance.Yacob.

Resolved! Timer of 10 Milliseconds

I want to configure timer of 10 millisecondsso for that according to calcuationUPDATE Frequency = TIMCLK / ((PSC+1) * (ARR+1))   My clock frequency is 108 MHzso when i set prescaler is 107 and ARR value is 9999 it should be updated frequcy is 100 H...

STM32F205 - UART5 Interrupt handler fail to receive interrupt

Hi all, Thanks for the support and sharing the experience.I have generated the code using STM32 CubeMx and using UART5 in interrupt mode. UART5 interrupt is configured to receive interrupt for every 1byte of data reception. Snap of the code is below....

DA.1115 by Associate II
  • 2737 Views
  • 5 replies
  • 0 kudos

Setting RTC Alarm for 1 Year from now

Hi,Is it possible to set the RTC Alarm (on STM32L496VG) to wake from low power for a specific date from now?For example 1 year from now or 10 years from now?Thanks for your help!

deckhard by Associate III
  • 1670 Views
  • 3 replies
  • 0 kudos

how do i program stmf105r8t6?

I am working on stm32f105r8t6 microcontroller. I need the pinout for this one. The data sheet that I found for this microcontroller doesn't show any of the pins that I need to program this microcontroller. It also doesn't show the RX/TX pins. Where c...

I have an existing product that uses a STM32F071CBT6 MCU. I want ad WiFi capability to the product. I was going to use the SPWF04S for this application but then I read that it is being phased out. Does STMicroelectronics

STMicroelectronicsSTM32F071CBT6I have an existing product that uses a STM32F071CBT6 MCU. I want ad WiFi capability to the product. I was going to use the SPWF04S for this application but then I read that it is being phased out. Does STMicroelectronic...

CStow.1 by Associate
  • 767 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.