STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Run MCU at Full Speed

Hi.I want to use my MCU at its max Speed.I am using STM32F103C8T6( Blue Pill ).Can any one Provide good resource?can anyone Provide source code for this ?Can anyone tell me about that in my Controller Why are we using RCC_CFGR and RCC_CFGR2?What is t...

CAN Bus error frame - how do I detect it [STM32]

What registers do I look at and what bits? Also, does the peripheral library wrap all the code needed to handle error frames? We are using a board Nucleo-G474RE.This question was already asked at https://community.st.com/s/question/0D50X00009XkhBe/ca...

Resolved! Step 2, LED Blinking with STM32F769I-Discovery

Dear community,I am totaly new and trying to get some idea on STM32F7...boardI've got opened an example project, provied within IDE. If I compile code and download it to MCU, everything works fine: 2 LEDs are blinking:This is the main code for LEDs b...

0693W000000U4dvQAC.png
IvanS by Associate II
  • 9403 Views
  • 8 replies
  • 0 kudos

Sample code

Hi!I'm an intern working with STM32L476 MCU. I am new to embedded system coding and was hoping to use a sample code as reference? is there any library where I can access some sample code?

Divya by Associate II
  • 2141 Views
  • 3 replies
  • 0 kudos

How NMI in STM32 works? How to trigger this interrupt?

Can you explain me how to trigger NMI in STM32F103 MCU? I am wondering what is the purpose of this interrupt? And Why it is called interrupt because interrupts are trigger by peripheral.Can you show me an example how to trigger it?Thanks so much

sholojda by Associate III
  • 9297 Views
  • 5 replies
  • 0 kudos

Resolved! Are the WLCSP versions of the STM32G4x3 and STM32G4x4 lines still on schedule to be released in Q1 2020, in light of the covid-19 situation?

@Imen DAHMEN​  Still looking here for a small-footprint solution in the stm32g4 line with hardware SPI flash (QuadSPI) handling. The WLCSP versions of the STM32G4x3 and STM32G4x4 lines might be viable. They are slated to be released in Q1 2020 (that ...

TB by Associate III
  • 1517 Views
  • 2 replies
  • 0 kudos

STM32F439 SDIO DMA CMD Response Timeout

Hello guys, I'm using a STM32F439 Board and try to use FatFS together with a SDIO (eMMC). Additionally I try to read and write with DMA. Now I generated a very big text file and want to write this on the eMMC. The file will be transmitted via Etherne...

AWied.1 by Associate II
  • 1971 Views
  • 2 replies
  • 0 kudos

Resolved! Please Help!! Why am I not able to setup ADC on STM32F030?

I am trying to setup the ADC channel on PA0. I have first set the pin mode to additional function. Then I have followed the examples provided in the reference manual. However, it doesn't turn on anything, either the calibration or the enable. It is n...

KHe.1 by Associate II
  • 2069 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.