STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L051 Stop Mode and LPTIM interrupt

I use HAL to go to STOP mode with interrupt (WFI), but the microcontroller immediately exits stop mode.I have LPTIM setup with HAL_LPTIM_Counter_Start_IT() to give interrupt after a few seconds, but even without setting up LPTIM I can't get the micro...

0693W000000Uh88QAC.png

STM32F429: Can Flash Sector "write protection" be set and temporarily cleared during operation (to erase or write some data)?

Hi AllI have been experimenting with the Flash write protection most of the day and was hoping to be able to set it by just writing the setting in the FLASH_OPTCR register, however the value that is written doesn't seem to affect anything unless comm...

hpipon957 by Associate III
  • 3576 Views
  • 5 replies
  • 0 kudos

Timers, How to set the timer ? In STM32 Please explain me. Watch my video I am explaining Timer multi tasking concept https://www.youtube.com/watch?v=EYXbNmaPBWo My Timer explanation in PIC 8 bit https://www.youtube.com/watch?v=dP1S4p7a1js

In Stm32 has too many parameters, So please some explain me how to use this ?. please watch my timer videos. because I know how to use the timer in PIC, but in stm32 which is prescalar and how to calculate for generating pulse(in expected frequency)

STM32 debugging issues.

I have been using STM32L010K8T6 with a J link debugger. It has been working good for past month or so. But now whenever I use a breakpoint the system does not stop at that particular break point or sometimes does not reach the break point at all. I t...

ARai by Associate II
  • 3953 Views
  • 5 replies
  • 0 kudos

STM32F4 - How do I switch a pin from ADC to normal GPIO mode?

Greetings all,I'm using the HAL libs to set a couple of pins for ADC use (one-shot).Later on during fw execution, i need to flip some of these pins back to normal GPIO mode.How do I do this?I've been looking over the programming manual, and HAL/LL li...

mwp by Senior
  • 1931 Views
  • 2 replies
  • 0 kudos

Microcontroller programming technology

Hello. Please tell us how the microcontroller programming process works. The controller can be programmed in two ways, fill the firmware through the bootloader and through the programmer.If in the first case there is microcode on the controller that ...

k.s.corp by Associate II
  • 2202 Views
  • 4 replies
  • 1 kudos

Resolved! Can't deference memory mapped qspi

I am using memory mapped mode of the QSPI peripheral on an STM32L452. I can see in the memory view at address 0x90000000 the bytes i expect. However, when dereferencing the pointer to that memory all i get is 0xFF's. In the attached photo you can see...

dan0 by Associate II
  • 2796 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.