STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F0 input capture interrupt quirk

Bare-metal STM32F030C8.Using input capture to receive encodes.Encodes are delimited by idle.I need to decode only the last 10 or so transitions of each encode.I want to perform the decode during the idle.So I’m using circular DMA and I want the timer...

alister by Lead
  • 17161 Views
  • 45 replies
  • 0 kudos

Variable PWM duty cycle signal on STM32F4

Hello everyone!For last week I am struggling to use Variable PWM duty cycle to generate signal for an array of addressable LEDs (WS2812) which I had successfully running on STM32F103.I was forced to use STM32F412 and ever since I cannot port my old c...

PPiro.1 by Associate II
  • 6667 Views
  • 11 replies
  • 0 kudos

Resolved! How to know which GPIO Pin to use for Timer Input Capture?

If I'm using a timer in input capture mode, how do I know which pins it wants to use for channels 1 and 2? I've been through the manual a bunch of times, looked for examples and other posts etc, I can't find the answer to this seemingly simple questi...

SWill.11 by Associate II
  • 3626 Views
  • 2 replies
  • 0 kudos

printf usage in stm32

Hi,I am using printf for my application to debug the output using UART.But I am facing the problem. void StartSender1(void const * argument)   {   /* USER CODE BEGIN 5 */ /* Infinite loop */ for(;;) { printf("Sender1 Sending\n"); osMessagePut(Queue...

Kumar B by Associate II
  • 2479 Views
  • 2 replies
  • 0 kudos

Problem with boot while programming stm32f407 mcu

I have a boot problem with the STM32F0407VGT6 (uVision V5.14.0.0.). I designed a custom board and sadly forgot to connect the Boot0 (floating) to GND. Because of that, I can program the MCU, but the controller don’t starts my program by default until...

FRJ.1 by Associate II
  • 2812 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.