STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

PKA - ecdsa curve support

The sample code uses p256v1 (which seems to actually be p256r1). This curve works well.​I Got PKA to sign correctly using p256k1 with some minor curve updates.​I​ am having trouble setting up p224r1. Has anyone got curves other that p256 to work?​T​n...

Hedley by Associate III
  • 3011 Views
  • 2 replies
  • 0 kudos

STM32L476RG not using flashed design

I just purchased the NUCLEO-STM32L47RG, and have tried using the following code below to press a switch to turn an LED on. However the code doesn't seem to actually be loading onto my microcontroller, I'm using Keil uVision 5 IDE if that makes a diff...

kfg4 by Associate
  • 1236 Views
  • 1 replies
  • 0 kudos

RTC runs slower 2 second / 5 minutes after disconnect power

We are using LSE 32,768. RTC looks like runs correctly if power is on. But if we disconnected power, RTC still hold data but run slower, about 2 seconds / 5 minutes.We changed new battery, even used power supply to feed vbat pin, same issue.I tried ...

Dat Tran by Senior II
  • 1912 Views
  • 3 replies
  • 0 kudos

Correctly programming I2C1 interface for STM32L151R8T6.

I'm trying to program i2C1 interface of STM32L151 with 3-rd side tools - Algocraft WN programmer.The sequence of operations attached in the DOC file.After these operations the START bit does not generated (checked by scope) and MASTER bit doesn't app...

LKuri.1 by Associate II
  • 4340 Views
  • 6 replies
  • 0 kudos

Use STM32H7 ETM without debugging tool

I need to use the ETM on a STM32H753 but without debugging tool. The idea is to record the execution trace all the time, and when the firmware encounter a critiical issue, output the trace to an external tool or program it to flash for later analysis...

Gpeti by Senior II
  • 11874 Views
  • 24 replies
  • 1 kudos

Resolved! STM32F4xx Rework of HAL CAN driver: examples?

Posted on February 01, 2018 at 21:39Hello!The HAL CAN driver for the STM32F4 got reworked lately (december 2017). I try to port my code from the old to the new drivers (compatibility break). There is a brief driver description in the update history ...

I need a timer to change its frequency every millisecond.I'm controlling a AC synchronous servo with pulse and direction in velocity mode(by changing the frequancy of the pulse) what is the ideal way

I have stm32f4 discovery board(STM32F407VGT06) running at 168Mhz. requirement 1) i have to run a motor (AC synchronous servo - yaskawa ) by pulse and direction.for which i can use a timer in PWM mode with 50% duty cycle. relat...

vsk.1 by Associate II
  • 3538 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.