STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! GPIO pin does not stay high

Hi everyone,I am trying to use CubeMX and the HAL library to get two STM32F411E discovery boards to communicate with each other via SPI. In a first step I am simply trying to configure the master correctly. I want to drive the NSS pin of the slave wi...

BKölz.1 by Associate
  • 4810 Views
  • 4 replies
  • 0 kudos

Resolved! STM32L43KC: Changing Clock Frequency?

Hey guys, just having the hardest of times changing clock frequency to 80MHz for the system clock and 43MHz for the ADC clock. Every time I try it seems the writing function to registers gets disabled such as RCC->AHB2ENR trying to enable GPIOA and A...

CLeo.1 by Senior II
  • 1897 Views
  • 5 replies
  • 1 kudos

Resolved! WFE examples required for stm32 family?

Hello ,I would like to get some examples for WFE based sleep . In stm32cube examples, i see that most of them are like WFI based examples. Request someone to help me with this information. Thanks in advance.Regards,Vinoth

STM32H745 DMA Mem-to-Mem inter-core data transfer

I would like to perform DMA based memory to memory transfer between cores with interrupt generation on Transfer Complete. To start of with the project i used Demo code (STM32Cube_FW_H7_V1.7.0 -> Projects -> NUCLEO-H745ZI-Q-> Demonstrations) added mem...

Madhan by Associate II
  • 1396 Views
  • 1 replies
  • 0 kudos

License talk

​After playing around with CubeMX for a while and looking at the generated code and at the SLA0044 Ultimate Liberty Lisence where ofcourse the question comes to mind what ultimate liberty... really means while there is a license that comes with it......

Resolved! Bare metal STM32F767 proper powering

HelloThis is my first time soldering a MCU on a custom PCB.As you know, STM32f767 is a very complicated chip and requires Vdd and Vss on many pins. Datasheet also states that capacitors are mandatory on each Vdd or Vref+. However Vref and Vdd (marked...

0693W000000Wm87QAC.png 0693W000000Wm82QAC.png
hashtala by Associate II
  • 1904 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.