STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Lcd EA_dogs 102 with stm32f091Rc nucleo board Hi everyone! I want to configure LCD with stm32f0 . I have the following code but it didn't work. Can you please help me.

#include "lcd.h" #include "font_lcd.h" #include "stm32f0xx.h" #include "stm32f0xx_conf.h"     // *********************************************************************** // Schreiben eines Zeichens an das LCD-Modul // seriell Soft-SPI Mode, 3/4 Draht ...

Nmo.1 by Associate III
  • 1718 Views
  • 2 replies
  • 0 kudos

Resolved! How to program FLASH_OPTR register to survive system reset?

Hello,I'm trying to control the boot behavior of my STM32L412 development board which has a floating BOOT0 hardware pin.I'm trying to clear the SWBOOT0 bit in FLASH_OPTR using firmware. So far I am able to unlock the register and clear the bit. Th...

GKerc.1 by Associate II
  • 5058 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F3 Comp not writing to registers

Hi All,So I've beern trying to write to the registers of the comparator 2 but when I debug , the values of the registers don't change. This leads me to believe that I have an issue getting the clock to the peripheral.I have a 16 MHz external XTAL whi...

glenn0010 by Associate III
  • 1227 Views
  • 3 replies
  • 0 kudos

elf flash fail after mass erase

I'm trying to debug an error I get when I try to flash internal flash on my stm32f4 board. I first use the flash_erase command to do a mass erase using openocd: flash erase_address unlock 0x08000000 0x100000Then use the flash_write command to flash t...

Rmo.1 by Associate
  • 842 Views
  • 0 replies
  • 0 kudos

I can't initialize stmpe811.

Hi, I'm working on a project with STM32F746 MCU and I used stmpe811 for touch controller but my code always going into hard fault error during initialization. I attached my project on the drive also I added the initialization part of code. Please hel...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.