STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Problem getting CLK and MOSI on SPI1 using STM32F091.

Hi there,Variations of this question have been asked before, but I have had no luck so far.I am attempting a very simple setup where I am using SPI to write to a display, where the screen does not talk back. I am using SPI1 on the STM32F091 and canno...

0693W000001rJTgQAM.png 0693W000001rJTqQAM.png 0693W000001rJUUQA2.png 0693W000001rJUoQAM.png
MFord.1 by Associate III
  • 3044 Views
  • 8 replies
  • 0 kudos

Resolved! Help me understand how to fix this issues with ADC scan feature

Hello,I'm using a STM32G431 MCU ADCs in dual mode. I'm trying to get control of the sampling rate and have found a frustrating issue. I don't need to scan multiple channels. Though the only way to get maximum sampling rate, or to have any control ove...

sd.1 by Associate II
  • 2892 Views
  • 3 replies
  • 0 kudos

Transfer Error (invalid Data) with USART1 & DMA

Hello,I setup USART1 using DMA with a STM32G071 & using HAL lib.Currently, i try to send uint8_t TxBuffer[7]={0x16,0x07,0x98,0x09,0x00,0x00,1B}.Transfert is done using HAL_UART_Transmit_DMA(&huart1, &TxBuffer[0], 7) and i have well manage the require...

RBarr.1 by Associate II
  • 2270 Views
  • 4 replies
  • 0 kudos

No 2020 STM32 wishlist

This is probably the promised replacement.[Edit 2023] Link above lead to Ideas, a section mostly ignored by ST (TouchFX crew being exception) and ultimately removed together with content i.e. user wishes when migrating to Khoros [/EDIT] Pity. It's be...

Resolved! Can anyone tell me how to configure external interrupts on stm32f103c8t6? is there anything wrong, my IRQHandler is not functioning properly...(actually, i wanted my LED(PA1) to glow when i interrupted it with push button(PB3) but it is not doing so...?

#include "stm32f10x.h"void EXTI3_IRQ_IRQHandler(void){ if(EXTI->PR & EXTI_PR_PR3) { EXTI->PR |= EXTI_PR_PR3; GPIOA-> BRR |= GPIO_BRR_BS1; }}int main(void){ RCC ->APB2ENR |= RCC_APB2ENR_IOPAEN;   //LED(OUTPUT PIN)(PA1) GPIOA->CRL &= ~(GPIO_CRL_CNF1); ...

Is it possible to use Serial SRAM (QSPI) with the STM32H743?

Hi allI have a custom Board with STM32H743 and i would like to add external SRAM and NOR Flash at the QSPI Interface. For example the SRAM at the Bank1 and the Flash at Bank2.Is this possible?I' would like to use for SRAM:https://www.mouser.ch/Produc...

RemoF by Associate
  • 2640 Views
  • 3 replies
  • 0 kudos

Generate PWM N-Pulses with each different Pulse width

We need to trigger camera by using PWM with different trigger delay for each photo. i.e trigger the camera at 100ms, 120ms, 150ms, 200ms, 210ms, 240ms, 260ms, 280ms, 300ms, 350ms for taking 10 photos at each cycle and this cycle repeats. Is it pos...

TShet by Associate II
  • 3573 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.