STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SFDC test question

<code><p>Hi everyone.</p><p> </p><p>So my previous post just did not load for some reason.</p><p>The problem is that for some reason I get this issue when I debug once I enable the interrupts.</p><p>I am simply trying to respond on the TIM5 interrupt...

CTest.1 by Associate
  • 693 Views
  • 0 replies
  • 0 kudos

Issue Programming STM32F04 through SWD

Hi all, I am trying to program the flash memory in my STM32F04 processor. I am doing this over SWD from another processor. I can successfully read all the DAP IDs etc and I also have figured out how to read and write from registers inside the stm32. ...

EOCon.1 by Associate II
  • 1465 Views
  • 2 replies
  • 0 kudos

Flash erase and write is not consistent in STM32G030K8.

Hello, I am using STM32G030K8 for my application. So, due to bug in my code, out of bound flash memory address was tried for write and hardfault occured. But after resolving bug and resetting MCU, I observed that flash erase and write is no...

OInam by Associate II
  • 1496 Views
  • 3 replies
  • 0 kudos

STM32F7 FMC SDRAM wrong reads

Hello,we have a STM32F7 interfaced to a CY62148EV30 SRAM with FMC bus.Sometimes, when several consecutive reads are performed, a wrong value is read.The wrong value has one or more bits at 0 instead of 1 (example: 0x52 is read instead of the correct ...

FMagg.1 by Associate
  • 808 Views
  • 0 replies
  • 0 kudos

STM32 PWM to stop after n pluses

Is there a way to stop STM32 PWM after 10 pluses ?I know one solution is using the system time and issue a stop via the code, however my issue is the stm CPU might be very busy to handle the stop signal.

Wleon.1 by Associate II
  • 5368 Views
  • 19 replies
  • 0 kudos

SWD Pins on STM32L476RG

Instead of using JTAG, I would like to enable SWD programming (via STLink) for a custom STM32L476RG board that I am designing. Which pins of the MCU correspond to the 5 SWD pins normally found on boards like Nucleo and Sensortile? I probably found ou...

SSaha.1 by Associate III
  • 1472 Views
  • 2 replies
  • 0 kudos

HAL_IWDG_Refresh causing the MCU to crash

I have my prescaler set to IWDG_PRESCALER_256 and Reload set to 16000Far before that counts down to 0 when I call HAL_IWDG_Refresh the program crashes.I am running on an STM32L072CZTAny ideaS?

Cfaya.1 by Associate II
  • 1394 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.