STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

memcmp crashes when accessing data stored in flash

STM32H745ziI am storing some configuration data in flash memory at address 0x080E0000.If I call HAL_FLASHEx_Erase and then do a memcmp of 24 bytes at this address vs a buffer where I have prepared data I want to write there everything is fine althoug...

KWest.1 by Associate II
  • 2408 Views
  • 3 replies
  • 0 kudos

Resolved! i would like to know how linker commands can be used in source file to push the multiple structure defines into a part of code memory. can some body share with examples

steps i tried.step 1: created a section in linker file ".parambuf"step2: in source file declared a structuretypedef struct{ param_t param[256]; \} t_param_block_t;step 3: in header files using attributes commands to push into parambuf section.extern ...

Anand Ram by Associate III
  • 1259 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F7 + QSPI (QUADSPI): Sporadic failure with memory-mapped flash memory. Disabling timeout does not help.

Hi everyone,We have an issue when using QUADSPI (memory-mapped) on a STM32F7 microcontroller. The controller sporadically runs into a watchdog reset. Investigation showed that the crash always occurs during a LDM instruction from the memory-mapped fl...

auraner by Associate II
  • 4919 Views
  • 6 replies
  • 0 kudos

Resolved! What STM32 Microcontroller will fit me

I am trying to make the transition from Arduino/Atmel micro controllers to something that can support true threading/multitasking in the 32bit ARM processor category. I am making a robot where I need to control 7+ 12v motors, 24 servos, 100+LEDS, spe...

ENoot.1 by Associate II
  • 6380 Views
  • 6 replies
  • 0 kudos

Problem Porting TLS CLient from F207 to H743

I managed to get a simple TLS client working on the NUCLEO-F207ZG. I cannot get the program to run on the NUCLEO-H743ZI2. On Wireshark I see several DHCP DISCOVER messages go out; followed by an OFFER message coming back. My code never responds with ...

Do SPI pins ever float?

When I used buffers between CPU and SPI peripherals I got problems. There were no Pull-ups.Bare GPIO pins with pull ups work. So do SPI pins float between transfers?CPU happens to be STM32H750/STM32F746 if it matters.

LMI2 by Lead
  • 2157 Views
  • 4 replies
  • 0 kudos

Resolved! Why is my SPI slave only sending one byte?

I am trying to read the position of an absolute rotary encoder (AMT22B-V). I have it connected to a Nucleo G474RE board. In the main.h file of the STM32CubeIDE project, I have the following declaration:#define BUFFERSIZE            (COUNTOF(aTxBuffer...

0693W000001ryUzQAI.png
MSzos.1 by Associate II
  • 3301 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.