STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Triggering ADC1 from TIM2 CH2 on stm32F767

Hi guys, I've searched the forum and found a handful of posts with a similar issue but the search doesn't seem to be very good for seeing previous posts... Anyway, I've got a PWM output from TIM2 CH1 (200us perioud, 25% D.C.) and I have another PWM f...

0693W000001sMM6QAM.png 0693W000001sMM1QAM.png
CDyer.1 by Senior
  • 1956 Views
  • 3 replies
  • 0 kudos

LPTIM1 vs TIM6 - low power

According to STM32L052K8 datasheet in table 39 page 72 of this document:https://www.st.com/resource/en/datasheet/stm32l052k8.pdfThose timers consume uA/MHz:Peripheral | Range 1 | Range 2 | Range 3 | Low-power sleep and runLPTIM1: 10, 8.5, 6.5, 8TIM6:...

godmode2 by Associate II
  • 2033 Views
  • 3 replies
  • 0 kudos

Pin Function Document

Hello,I'm using the NUCLEO-F722ZE EVB.In page 43 of the following document there seems to be a pinout list which specifies the signal name of each pin :https://www.st.com/resource/en/user_manual/dm00244518-stm32-nucleo144-boards-stmicroelectronics.pd...

skon.1 by Senior
  • 2064 Views
  • 4 replies
  • 0 kudos

What does the internal temperature sensor measure?

We are using an STMF4 and STMF3 in our product and are trying to see if we need to switch to the industrial variant for the extended temperature range.? Is the internal temperature sensor measuring the Die temperature, and if so is that essentially ...

PCicc.1 by Associate
  • 1404 Views
  • 2 replies
  • 0 kudos

Is it possible to stop ADC-DMA transfers when debugging?

I have an ADC1 setup in continuous mode and DMA1 in circular mode setup to transfer adc data to a circular buffer in memory. The data is processed directly from the circular buffer and the buffer is big enough that the processing is done before the b...

Fibo by Associate II
  • 2940 Views
  • 2 replies
  • 0 kudos

Will dividing down an external clock add jitter?

I read in the general timer manual for the STM32 (AN4013) that the external clock inputs (ETR, TI1, and TI2), which can be used for timer inputs, are synchronized internally with the APBx clock.I just want to make sure I am understanding this correct...

Use the CAN with the F469-Discovery

It's possible to use the CAN with the STM32F469I-Discovery?I have saw that the CAN1 pins are used for the touchscreen (I2C), so i can't use it. I can use the CAN2, but it's a slave on the STM32F469.  I have read that if I want to use the CAN as a sla...

Luca1 by Senior
  • 1742 Views
  • 2 replies
  • 0 kudos

Resolved! I need to be able to count pulses that are incoming on a GPIO. What is the best way to do this? Timers?

I have an application where I need to count the total number of pulses coming in from a fuel flow sensor. I then take the total number of pulses to display a readout of the total amount of fuel that has flowed through the sensor since the counter beg...

NChal.1 by Associate II
  • 4998 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.