Resolved! Restart MCU via software
Hi, How can I restart stm32l431 via software? I an using the MCU with sim800l and I can be able to restart MCU using text message. Does Exist some HAL function to restart MCU?
Ask questions, find answers, and share insights on STM32 products and their technical features.
Hi, How can I restart stm32l431 via software? I an using the MCU with sim800l and I can be able to restart MCU using text message. Does Exist some HAL function to restart MCU?
Hi,I just order some stm toolkit from eStore and my question is where is order status ?? https://www.st.com/content/st_com/en/sample_and_buy/sample-and-buy/buy-from-estore.html
Hi all!Been a loooong time since I've been around forums, but I'm back!So a long time project I've wanted to do is coming back into my brain and I figure its time to start chipping away at it!I love RGB LEDs, especially the addressable variety, and I...
I'm trying to send some data from master to a slave (the STM32F103C6) with HAL functions, with HAL_I2C_Slave_Receive() -no interrupt mode- the reception works flawlessly but with HAL_I2C_Slave_Receive_IT() -the one needed- the slave acknowledges its ...
Hello,I setup i2c1 as per below. I am trying to get data from a MPU6050 device on I2C but I got error code 4.On the same hardware I tested using Arduino IDE and I can read data from MPU without problems.Can one support please guide me where should I ...
Hi, I have never work with register. I need to restart counter of LPTIM in stm32l431. The documentation says that I need to set a register to '1'. The image explain this. How I can do that? Thank's a lot.
Hi,I am trying to enable DCache on a USART Tx DMA snippet, which causes USART Tx to fail.The impression that I have is that the MCU has already written to physical memory and the DMA should have no trouble in accessing the written memory ?Can someone...
Hello guys, I am working on a acoustic source localization project. I need to sample the amplified signal from Hydrophone. The acoustic source emits a sound frequency of 42khz. I need to sample this signal at a frequency of 100Khz or even 200khz(if p...
Hello,Which mcu products are provided as dies or wafer?Thanks
Hi Everyone,My problem relates to I2C communication when trying to send bytes to a display on address 0x78. First I tried with the plain I2C HAL function(blocking), but I realised that the MCU gets frozen because of the huge amount of data to be sent...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.