STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Data bits shifted in SPI communication on STM32L462 after repeating one successful session (consisting of NSS falling edge, 3 separated transmissions with HAL_SPI_TransmitReceive, NSS, rising edge)

Data bits are shifted on second SPI session (BSY bit stay high at the end of data transfer in slave mode) We are using STM32L462VET6, and initialize SPI2 in full duplex slave mode (CPOL=1, CPHA=2-edges) with software NSS and baudrate 960 kHz with HCL...

YVido.1 by Associate
  • 1975 Views
  • 3 replies
  • 0 kudos

Facing issue while sending data through UDP broadcast using B-L45E-IOT01A1 board with WiFi firmware revision C3-5.2.5

I am using the board B-L475E-IOT01A1. I want to send data via UDP broadcast.I have a udp server running on a host at port 1100I use the following set of AT commands to open a Client Connection after initializing the WiFi module and connecting it to a...

PMaha.1 by Associate II
  • 840 Views
  • 0 replies
  • 0 kudos

Resolved! stm32 lowpower run mode comsuption

debug a program in the sram, the current is 29 uA, how to down to 8uA or lower ?i dont know how to disable flash/eeprom or other peripheral

Staly.1 by Associate III
  • 2577 Views
  • 5 replies
  • 0 kudos

RTC in Hardware Layout

I am going to use RTC in my application to generate time stamps. I am currently using Nucelo - L412KB evaluation module. Do I need to connect any pins or add any components? Where can I find this information?

Anonymous by Associate II
  • 1734 Views
  • 2 replies
  • 0 kudos

SPI output is wrong

I have STM32F407 that is communicating with TFT lcd over SPI. What I am seeing with Logic Analyzer doesnt match what I am sending. I cant see the pattern, but data is consistent, so its probably some setting that is off. I tried all combinations of C...

Gossamer by Associate II
  • 1343 Views
  • 5 replies
  • 0 kudos

Problem with Flash_Write after a reset

Hi,I'm using the FLASH_Write function in order to save a table in a specific address. Once it is saved correctly I reset the board and try to change another address with the same function.The problem is that the flash_write function works at the firs...

Moughit by Associate III
  • 2345 Views
  • 2 replies
  • 0 kudos

I2C SDA abnormal

When I used the STM32L412KB as an I2C slave. when there only one slave on the bus, all the function works well. but if there hastwo devices on the bus and continue to access one slave device, the non-addressed I2C slave will damage the SDA bus. I cap...

Haifeng by Associate II
  • 2727 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.